CollisionMaterialCollection Class¶
-
class
NXOpen.Mechatronics.
CollisionMaterialCollection
¶ Bases:
object
Represents a collection of Collision Material.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateCollisionMaterialBuilder | Creates a NXOpen.Mechatronics.CollisionMaterialBuilder . |
FindObject | Finds the NXOpen.Mechatronics.CollisionMaterial with the given name. |
Method Detail¶
CreateCollisionMaterialBuilder¶
-
CollisionMaterialCollection.
CreateCollisionMaterialBuilder
¶ Creates a
NXOpen.Mechatronics.CollisionMaterialBuilder
.Signature
CreateCollisionMaterialBuilder(collisionMaterial)
Parameters: collisionMaterial ( NXOpen.Mechatronics.CollisionMaterial
) –NXOpen.Mechatronics.CollisionMaterial
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.CollisionMaterialBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
CollisionMaterialCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.CollisionMaterial
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.CollisionMaterial
.Returns: NXOpen.Mechatronics.CollisionMaterial
with this name.Return type: NXOpen.Mechatronics.CollisionMaterial
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)