CollisionMaterialBuilder Class¶
-
class
NXOpen.Mechatronics.
CollisionMaterialBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.CollisionMaterial
builder.To create a new instance of this class, use
NXOpen.Mechatronics.CollisionMaterialCollection.CreateCollisionMaterialBuilder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
DynamicFriction | Returns the dynamic friction. |
Name | Returns or sets the name. |
Restitution | Returns the restitution. |
RollingFriction | Returns the rolling friciton. |
StaticFriction | Returns the static friction. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DynamicFriction¶
-
CollisionMaterialBuilder.
DynamicFriction
¶ Returns the dynamic friction.
-------------------------------------
Getter Method
Signature
DynamicFriction()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Name¶
-
CollisionMaterialBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Restitution¶
-
CollisionMaterialBuilder.
Restitution
¶ Returns the restitution.
-------------------------------------
Getter Method
Signature
Restitution()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RollingFriction¶
-
CollisionMaterialBuilder.
RollingFriction
¶ Returns the rolling friciton.
-------------------------------------
Getter Method
Signature
RollingFriction()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StaticFriction¶
-
CollisionMaterialBuilder.
StaticFriction
¶ Returns the static friction.
-------------------------------------
Getter Method
Signature
StaticFriction()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
CollisionMaterialBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.