ChangeMaterialBuilder Class¶
-
class
NXOpen.Mechatronics.
ChangeMaterialBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
Represents a
NXOpen.Mechatronics.ChangeMaterial
builder.To create a new instance of this class, use
NXOpen.Mechatronics.ChangeMaterialCollection.CreateChangeMaterialBuilder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
CollisionMaterial | Returns or sets the material. |
FirstBody | Returns the first body of collision pair. |
Name | Returns or sets the name. |
SecondBody | Returns the second body of collision pair. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetFirstBody | Sets the first object. |
SetSecondBody | Sets the second object. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CollisionMaterial¶
-
ChangeMaterialBuilder.
CollisionMaterial
¶ Returns or sets the material.
This can be
NXOpen.Mechatronics.CollisionMaterial
.-------------------------------------
Getter Method
Signature
CollisionMaterial()
Returns: Return type: NXOpen.Mechatronics.CollisionMaterial
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
CollisionMaterial(collisionMaterial)
Parameters: collisionMaterial ( NXOpen.Mechatronics.CollisionMaterial
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FirstBody¶
-
ChangeMaterialBuilder.
FirstBody
¶ Returns the first body of collision pair.
This can be
NXOpen.Mechatronics.RigidBody
,NXOpen.Mechatronics.CollisionBody
orNXOpen.Mechatronics.TransportSurface
.-------------------------------------
Getter Method
Signature
FirstBody()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SecondBody¶
-
ChangeMaterialBuilder.
SecondBody
¶ Returns the second body of collision pair.
This can be
NXOpen.Mechatronics.RigidBody
,NXOpen.Mechatronics.CollisionBody
orNXOpen.Mechatronics.TransportSurface
.-------------------------------------
Getter Method
Signature
SecondBody()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
SetFirstBody¶
-
ChangeMaterialBuilder.
SetFirstBody
¶ Sets the first object.
This can be
NXOpen.Mechatronics.RigidBody
,NXOpen.Mechatronics.CollisionBody
orNXOpen.Mechatronics.TransportSurface
.Signature
SetFirstBody(firstBody)
Parameters: firstBody ( NXOpen.DisplayableObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetSecondBody¶
-
ChangeMaterialBuilder.
SetSecondBody
¶ Sets the second object.
This can be
NXOpen.Mechatronics.RigidBody
,NXOpen.Mechatronics.CollisionBody
orNXOpen.Mechatronics.TransportSurface
.Signature
SetSecondBody(secondBody)
Parameters: secondBody ( NXOpen.DisplayableObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ChangeMaterialBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.