NXOpen.Issue.IssueAttachment |
Represents the Issue Attachment object. |
NXOpen.Issue.IssueBriefcase |
Represents the Issue Briefcase object. |
NXOpen.Issue.IssueBriefcaseSynchronizeBuilder |
Represents a NXOpen.Issue.IssueBriefcase synchronize builder |
NXOpen.Issue.IssueContent |
Represents the Issue Issue object. |
NXOpen.Issue.IssueContentBuilder |
Represents a NXOpen.Issue.IssueContent builder |
NXOpen.Issue.IssueFolder |
Represents the Issue Folder object. |
NXOpen.Issue.IssueList |
Represents the Issue List object. |
NXOpen.Issue.IssueListCollection |
Represents a NXOpen.Issue.IssueListCollection |
NXOpen.Issue.IssueManager |
Contains the collection objects for creating and iterating over issue objects. |
NXOpen.Issue.IssueProperty |
Represents the Issue Property object. |
NXOpen.Issue.IssueSite |
Represents the Issue Site object. |
NXOpen.Issue.SnapshotSubsetBuilder |
Used to create or edit issue snapshot subset. |
NXOpen.Issue.SnapshotWorksetBuilder |
Used to create or edit issue snapshot workset which is a container to hold all the corresponding parts to represent an issue. |