IssueBriefcaseSynchronizeBuilder Class¶
-
class
NXOpen.Issue.
IssueBriefcaseSynchronizeBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Issue.IssueBriefcase
synchronize builderTo create a new instance of this class, use
NXOpen.Issue.IssueBriefcase.CreateSynchronizeContentBuilder
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
AddPartAttachment | Adds an part type NXOpen.Issue.IssueAttachment , only the added parts can be synchronized to server. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
RemovePartAttachment | Adds an part type NXOpen.Issue.IssueAttachment . |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AddPartAttachment¶
-
IssueBriefcaseSynchronizeBuilder.
AddPartAttachment
¶ Adds an part type
NXOpen.Issue.IssueAttachment
, only the added parts can be synchronized to server.Signature
AddPartAttachment(attachment)
Parameters: attachment ( NXOpen.Issue.IssueAttachment
) –New in version NX10.0.0.
License requirements: nx_issue_mgmt (“NX Issue Tracking”)
RemovePartAttachment¶
-
IssueBriefcaseSynchronizeBuilder.
RemovePartAttachment
¶ Adds an part type
NXOpen.Issue.IssueAttachment
.Signature
RemovePartAttachment(attachment)
Parameters: attachment ( NXOpen.Issue.IssueAttachment
) –New in version NX10.0.0.
License requirements: nx_issue_mgmt (“NX Issue Tracking”)
Validate¶
-
IssueBriefcaseSynchronizeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.