InterpartExpressionsBuilder Class¶
-
class
NXOpen.
InterpartExpressionsBuilder
¶ Bases:
NXOpen.Builder
This class creates interpart expressions from the source part to the current work part via the naming rule defined.
To create a new instance of this class, use
NXOpen.ExpressionCollection.CreateInterpartExpressionsBuilder
Default values.
Property Value NamingRule AddPrefix New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
BaseString | Returns or sets the base string. |
NamingRule | Returns or sets the naming rule. |
ReplaceString | Returns or sets the replace string. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetExpressions | Get an array of source expressions. |
GetObject | Returns the object currently being edited by this builder. |
SetExpressions | Set an array of source expressions. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InterpartExpressionsBuilderNamingRules Enumeration | This defines the naming rule used for the name of the expression created in the current work part. |
Property Detail¶
BaseString¶
-
InterpartExpressionsBuilder.
BaseString
¶ Returns or sets the base string.
This string is used as the prefix for AddPrefix, the suffix for AddSuffix, the replaced string for Replace and the rename string for RenameWithIndex.
-------------------------------------
Getter Method
Signature
BaseString()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BaseString(baseString)
Parameters: baseString (str) – New in version NX8.5.0.
License requirements: None.
NamingRule¶
-
InterpartExpressionsBuilder.
NamingRule
¶ Returns or sets the naming rule.
This determines how the name of the expression in the current work part is constructed.
-------------------------------------
Getter Method
Signature
NamingRule()
Returns: Return type: NXOpen.InterpartExpressionsBuilderNamingRules
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NamingRule(namingRule)
Parameters: namingRule ( NXOpen.InterpartExpressionsBuilderNamingRules
) –New in version NX8.5.0.
License requirements: None.
ReplaceString¶
-
InterpartExpressionsBuilder.
ReplaceString
¶ Returns or sets the replace string.
This string replaces the BaseString for the Replace.
-------------------------------------
Getter Method
Signature
ReplaceString()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReplaceString(replaceString)
Parameters: replaceString (str) – New in version NX8.5.0.
License requirements: None.
Method Detail¶
GetExpressions¶
-
InterpartExpressionsBuilder.
GetExpressions
¶ Get an array of source expressions.
These are the source expressions to be referenced by the current work part. The destination names can be used to override the naming rule for a given source expression. This is a parallel array. Each source expression has an entry in this array for its destination name. If the associated destination name is the empty string then the naming rule will be used to generate the destination name for a given source expression otherwise the destination name itself will be used to name the new expression in the current work part.
Signature
GetExpressions()
Returns: a tuple Return type: A tuple consisting of (sourceExpressions, destinationNames). sourceExpressions is a list of NXOpen.Expression
. array of source expressions destinationNames is a list of str. array of destination namesNew in version NX8.5.0.
License requirements: None.
SetExpressions¶
-
InterpartExpressionsBuilder.
SetExpressions
¶ Set an array of source expressions.
These are the source expressions to be referenced by the current work part. The destination names can be used to override the naming rule for a given source expression. This is a parallel array. Each source expression has an entry in this array for its destination name. If the associated destination name is the empty string then the naming rule will be used to generate the destination name for a given source expression otherwise the destination name itself will be used to name the new expression in the current work part.
Signature
SetExpressions(sourceExpressions, destinationNames)
Parameters: - sourceExpressions (list of
NXOpen.Expression
) – array of source expressions - destinationNames (list of str) – array of destination names
New in version NX8.5.0.
License requirements: None.
- sourceExpressions (list of
Validate¶
-
InterpartExpressionsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.