ExpressionCollection Class¶
-
class
NXOpen.
ExpressionCollection
¶ Bases:
object
Represents a collection of expressions.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
AskInterpartLhsName | Returns the left hand side name for an overriding interpart expression reference. |
AskInterpartRhsName | Returns the right hand side name for an interpart expression reference. |
ChangeInterpartReferences | Changes all of the references in the part owning_part from expressions in the part old_part_name to expressions in the part new_part_name. |
Create | Creates an expression @return the new expression |
CreateExpression | Creates an expression of the specified type. |
CreateInterpartExpressionsBuilder | Creates interpart expressions. |
CreateReplaceExpressionsBuilder | Replace expressions. |
CreateSuppressByExpressionBuilder | Creates a NXOpen.SuppressByExpressionBuilder @return SuppressByExpressionBuilder object |
CreateSystemExpression | Creates a system expression. |
CreateSystemExpressionFromReferenceString | Creates a system string expression from a reference string in Drafting Note format. |
CreateSystemExpressionWithUnits | Creates a system expression with units. |
CreateWithUnits | Creates an expression with units. |
Delete | Deletes an expression |
Edit | Edits an expression. |
EditWithUnits | Edits an expression with units. |
ExportToFile | Exports the expressions to a text file, or, if ‘file_name’ is None, list the expressions in the listing window. |
FindObject | Finds the NXOpen.Expression with the given identifier as recorded in a journal. |
GetAttributeExpression | Get the attribute expression of the specified attribute title/type. |
GetInterpartReferences | Returns a list of parts that are referenced from expressions in the part owning_part. |
GetInterpartReferencesWithDisplayNames | Returns a list of parts that are referenced from expressions in the part owning_part. |
GetVisibleExpressions | Returns an array of visible Number expressions in the part. |
ImportFromFile | Imports expressions from a file. |
RemoveInterpartReferences | Removes the interpart references from a part. |
Rename | Changes the name of the expression. |
Replace | Replaces references to an expression with another expression. |
ReplaceAttributeExpression | Replace the attribute expression of the specified attribute title/type. |
SystemRename | Changes the name of the expression without marking system expressions as user expressions. |
Enumerations¶
ExpressionCollectionExportMode Enumeration | Indicates the mode for exporting expressions. |
ExpressionCollectionImportMode Enumeration | Indicates the mode for importing expressions. |
ExpressionCollectionSortType Enumeration | Indicates the mode for sorting expressions. |
Method Detail¶
AskInterpartLhsName¶
-
ExpressionCollection.
AskInterpartLhsName
¶ Returns the left hand side name for an overriding interpart expression reference.
Signature
AskInterpartLhsName(sourceExpression)
Parameters: sourceExpression ( NXOpen.Expression
) – expression in source partReturns: left hand side name Return type: str New in version NX10.0.0.
License requirements: None.
AskInterpartRhsName¶
-
ExpressionCollection.
AskInterpartRhsName
¶ Returns the right hand side name for an interpart expression reference.
Signature
AskInterpartRhsName(sourceExpression)
Parameters: sourceExpression ( NXOpen.Expression
) – expression in source partReturns: right hand side name Return type: str New in version NX10.0.0.
License requirements: None.
ChangeInterpartReferences¶
-
ExpressionCollection.
ChangeInterpartReferences
¶ Overloaded method ChangeInterpartReferences
ChangeInterpartReferences(oldPartName, newPartName)
ChangeInterpartReferences(oldPartName, newPartName, doUpdate, doChecking)
-------------------------------------
Changes all of the references in the part “owning_part” from expressions in the part “old_part_name” to expressions in the part “new_part_name”.
Signature
ChangeInterpartReferences(oldPartName, newPartName)
Parameters: - oldPartName (str) – Part name whose references are being replaced
- newPartName (str) – New part name to reference
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Changes all of the references in the part “owning_part” from expressions in the part “old_part_name” to expressions in the part “new_part_name”.
Signature
ChangeInterpartReferences(oldPartName, newPartName, doUpdate, doChecking)
Parameters: - oldPartName (str) – Part name whose references are being replaced
- newPartName (str) – New part name to reference
- doUpdate (bool) – Do update if true
- doChecking (bool) – Do checking if true
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Create¶
-
ExpressionCollection.
Create
¶ Creates an expression
Signature
Create(string)
Parameters: string (str) – the equation for the expression. Must be in the format: name = right_hand_side. For example, “x = 1.2 * y + z”. Returns: the new expression Return type: NXOpen.Expression
New in version NX3.0.0.
License requirements: None.
CreateExpression¶
-
ExpressionCollection.
CreateExpression
¶ Creates an expression of the specified type.
Signature
CreateExpression(expressionType, string)
Parameters: - expressionType (str) – The type of the expression, such as “Number”, “String”, “Boolean”, “Integer”, “Point” and “Vector”
- string (str) – the equation for the expression. Must be in the format: name = right_hand_side. For example, “x = 1.2 * y + z”.
Returns: the new expression
Return type: New in version NX5.0.0.
License requirements: None.
CreateInterpartExpressionsBuilder¶
-
ExpressionCollection.
CreateInterpartExpressionsBuilder
¶ Creates interpart expressions.
Signature
CreateInterpartExpressionsBuilder()
Returns: Return type: NXOpen.InterpartExpressionsBuilder
New in version NX8.5.0.
License requirements: None.
CreateReplaceExpressionsBuilder¶
-
ExpressionCollection.
CreateReplaceExpressionsBuilder
¶ Replace expressions.
Signature
CreateReplaceExpressionsBuilder()
Returns: Return type: NXOpen.ReplaceExpressionsBuilder
New in version NX10.0.0.
License requirements: None.
CreateSuppressByExpressionBuilder¶
-
ExpressionCollection.
CreateSuppressByExpressionBuilder
¶ Creates a
NXOpen.SuppressByExpressionBuilder
Signature
CreateSuppressByExpressionBuilder()
Returns: SuppressByExpressionBuilder object Return type: NXOpen.SuppressByExpressionBuilder
New in version NX5.0.0.
License requirements: None.
CreateSystemExpression¶
-
ExpressionCollection.
CreateSystemExpression
¶ Overloaded method CreateSystemExpression
CreateSystemExpression(string)
CreateSystemExpression(expressionType, string)
-------------------------------------
Creates a system expression. After creating a system expression, you should associate it with an object, such as a sketch dimension. System expressions are deleted when the object they are associated with is deleted.
Signature
CreateSystemExpression(string)
Parameters: string (str) – the equation or right-hand-side for the expression. You can specify a name for the equation by providing a string in the format: name = right_hand_side. For example, “x = 1.2 * y + z”. If you do not provide a name, a name will be assigned automatically. For example, if the string is “1.2 * y + z”, a name will be assigned automatically. Returns: the new expression Return type: NXOpen.Expression
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Creates a system expression of the specified type. After creating a system expression, you should associate it with an object, such as a sketch dimension. System expressions are deleted when the object they are associated with is deleted.
Signature
CreateSystemExpression(expressionType, string)
Parameters: - expressionType (str) – The type of the expression, such as “Number”, “String”, “Boolean”, “Integer”, “Point” and “Vector”
- string (str) – the equation or right-hand-side for the expression. You can specify a name for the equation by providing a string in the format: name = right_hand_side. For example, “x = 1.2 * y + z”. If you do not provide a name, a name will be assigned automatically. For example, if the string is “1.2 * y + z”, a name will be assigned automatically.
Returns: the new expression
Return type: New in version NX5.0.0.
License requirements: None.
-------------------------------------
CreateSystemExpressionFromReferenceString¶
-
ExpressionCollection.
CreateSystemExpressionFromReferenceString
¶ Creates a system string expression from a reference string in Drafting Note format.
Only expressions (X) and attributes (W) are supported.
Here is how the control character sequences need to be formatted: Expressions - Xm.n<@>exp_name Part Attributes - W<@>attr_title Object Attributes - W!obj_id<@>attr_title
Signature
CreateSystemExpressionFromReferenceString(reference)
Parameters: reference (str) – the reference string in Drafting Note format Returns: the new expression Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
CreateSystemExpressionWithUnits¶
-
ExpressionCollection.
CreateSystemExpressionWithUnits
¶ Creates a system expression with units.
After creating a system expression, you should associate it with an object, such as a sketch dimension. System expressions are deleted when the object they are associated with is deleted.
Signature
CreateSystemExpressionWithUnits(string, unitType)
Parameters: - string (str) – the equation or right-hand-side for the expression. You can specify a name for the equation by providing a string in the format: name = right_hand_side. For example, “x = 1.2 * y + z”. If you do not provide a name, a name will be assigned automatically. For example, if the string is “1.2 * y + z”, a name will be assigned automatically.
- unitType (
NXOpen.Unit
) – units for the expression
Returns: the new expression
Return type: New in version NX4.0.0.
License requirements: None.
CreateWithUnits¶
-
ExpressionCollection.
CreateWithUnits
¶ Overloaded method CreateWithUnits
CreateWithUnits(string, unitType)
CreateWithUnits(leftHandSide, rightHandSide, isUserLocked, units)
-------------------------------------
Creates an expression with units.
Signature
CreateWithUnits(string, unitType)
Parameters: - string (str) – the equation for the expression. Must be in the format: name = right_hand_side. For example, “x = 1.2 * y + z”.
- unitType (
NXOpen.Unit
) – units for the expression
Returns: the new expression
Return type: New in version NX4.0.0.
License requirements: None.
-------------------------------------
Delete¶
-
ExpressionCollection.
Delete
¶ Deletes an expression
Signature
Delete(expression)
Parameters: expression ( NXOpen.Expression
) – The expression to be deletedNew in version NX4.0.0.
License requirements: None.
Edit¶
-
ExpressionCollection.
Edit
¶ Edits an expression.
Note, there is no difference between this method and editing the expression via
NXOpen.Expression.RightHandSide
if the ExpressionCollection is owned by the part that owns the expression.Signature
Edit(expression, newRightHandSide)
Parameters: - expression (
NXOpen.Expression
) – The expression to be edited, Note: if this expression is not owned by the part that owns the ExpressionCollection, a new expression will be created in the part that owns the ExpressionCollection - newRightHandSide (str) – What you want to change the expression to
New in version NX3.0.0.
License requirements: None.
- expression (
EditWithUnits¶
-
ExpressionCollection.
EditWithUnits
¶ Edits an expression with units.
Changing the units on an existing expression is only allowed when the expression is not referenced yet.
Note, if you do not change the units, there is no difference between this method and editing the expression via
NXOpen.Expression.RightHandSide
if the ExpressionCollection is owned by the part that owns the expression.Signature
EditWithUnits(expression, unitType, newRightHandSide)
Parameters: - expression (
NXOpen.Expression
) – The expression to be edited, Note: if this expression is not owned by the part that owns the ExpressionCollection, a new expression will be created in the part that owns the ExpressionCollection - unitType (
NXOpen.Unit
) – units for the expression - newRightHandSide (str) – What you want to change the expression to
New in version NX4.0.0.
License requirements: None.
- expression (
ExportToFile¶
-
ExpressionCollection.
ExportToFile
¶ Exports the expressions to a text file, or, if ‘file_name’ is None, list the expressions in the listing window.
Throws an exception if there is any error.
NOTE: if the file already exists, an exception is thrown and the file is not overwritten.
Signature
ExportToFile(exportMode, fileName, sortType)
Parameters: - exportMode (
NXOpen.ExpressionCollectionExportMode
) – export mode - fileName (str) – File name specification to export expressions into.
- sortType (
NXOpen.ExpressionCollectionSortType
) – How to sort the exported expressions
New in version NX4.0.0.
License requirements: None.
- exportMode (
FindObject¶
-
ExpressionCollection.
FindObject
¶ Finds the
NXOpen.Expression
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Expression found Return type: NXOpen.Expression
New in version NX3.0.0.
License requirements: None.
GetAttributeExpression¶
-
ExpressionCollection.
GetAttributeExpression
¶ Get the attribute expression of the specified attribute title/type.
Signature
GetAttributeExpression(object, title, type, index)
Parameters: - object (
NXOpen.NXObject
) – The object of the attribute - title (str) – The title of the attribute
- type (
NXOpen.NXObjectAttributeType
) – The type of the attribute - index (int) – The array index if the attribute is an array (use -1 otherwise)
Returns: the attribute expression
Return type: New in version NX8.0.0.
License requirements: None.
- object (
GetInterpartReferences¶
-
ExpressionCollection.
GetInterpartReferences
¶ Returns a list of parts that are referenced from expressions in the part “owning_part”.
Signature
GetInterpartReferences()
Returns: array of part names Return type: list of str New in version NX4.0.0.
License requirements: None.
GetInterpartReferencesWithDisplayNames¶
-
ExpressionCollection.
GetInterpartReferencesWithDisplayNames
¶ Returns a list of parts that are referenced from expressions in the part “owning_part”.
Signature
GetInterpartReferencesWithDisplayNames()
Returns: a tuple Return type: A tuple consisting of (referencedPartNames, referencedDispNames). referencedPartNames is a list of str. array of internal part names referencedDispNames is a list of str. array of display part names New in version NX10.0.0.
License requirements: None.
GetVisibleExpressions¶
-
ExpressionCollection.
GetVisibleExpressions
¶ Returns an array of visible “Number” expressions in the part.
Signature
GetVisibleExpressions()
Returns: array of “Number” expressions Return type: list of NXOpen.Expression
New in version NX4.0.0.
License requirements: None.
ImportFromFile¶
-
ExpressionCollection.
ImportFromFile
¶ Imports expressions from a file.
Input a file specification. When calling this method, changes are not applied to the system until
Update.DoUpdate
is called.Signature
ImportFromFile(fileName, importMode)
Parameters: - fileName (str) – File name specification to import expressions from
- importMode (
NXOpen.ExpressionCollectionImportMode
) – import mode
Returns: a tuple
Return type: A tuple consisting of (expModified, errorMessages). expModified is a bool. TRUE if any expressions were affected by the import errorMessages is a list of str. translated list of error messages
New in version NX4.0.0.
License requirements: None.
RemoveInterpartReferences¶
-
ExpressionCollection.
RemoveInterpartReferences
¶ Removes the interpart references from a part.
If a part name is given, then it removes the references to that part. If part_name is None, it removes all references to all parts.
References on the RHS are replaced by a numerical value, References on the LHS are deleted. E.g.
x = comp::len + z –<ja_gt> x = 3 + z
comp::height=5 –<ja_gt> (deleted)
The function returns TRUE is any references were removed, and FALSE otherwise.
Signature
RemoveInterpartReferences(partName)
Parameters: partName (str) – Part name to remove references for Returns: whether any changes were made Return type: bool New in version NX4.0.0.
License requirements: None.
Rename¶
-
ExpressionCollection.
Rename
¶ Changes the name of the expression.
Signature
Rename(expression, newName)
Parameters: - expression (
NXOpen.Expression
) – expression to be renamed - newName (str) – new name of the expression
New in version NX4.0.0.
License requirements: None.
- expression (
Replace¶
-
ExpressionCollection.
Replace
¶ Replaces references to an expression with another expression.
Signature
Replace(currentName, replaceName)
Parameters: - currentName (str) – current expression name
- replaceName (str) – replace expression name
New in version NX10.0.0.
License requirements: None.
ReplaceAttributeExpression¶
-
ExpressionCollection.
ReplaceAttributeExpression
¶ Replace the attribute expression of the specified attribute title/type.
Signature
ReplaceAttributeExpression(expression, object, title, type, index)
Parameters: - expression (
NXOpen.Expression
) – the attribute expression - object (
NXOpen.NXObject
) – The object of the attribute - title (str) – The title of the attribute
- type (
NXOpen.NXObjectAttributeType
) – The type of the attribute - index (int) – The array index if the attribute is an array (use -1 otherwise)
New in version NX8.0.0.
License requirements: None.
- expression (
SystemRename¶
-
ExpressionCollection.
SystemRename
¶ Changes the name of the expression without marking system expressions as user expressions.
Signature
SystemRename(expression, newName)
Parameters: - expression (
NXOpen.Expression
) – expression to be renamed - newName (str) – new name of the expression
New in version NX6.0.0.
License requirements: None.
- expression (