SpinePointDataCollection Class¶
-
class
NXOpen.GeometricUtilities.
SpinePointDataCollection
¶ Bases:
object
This class contains the factory methods for creating a SpinePointData object.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateSpinePointData | Creates a SpinePointData object. |
Method Detail¶
CreateSpinePointData¶
-
SpinePointDataCollection.
CreateSpinePointData
¶ Overloaded method CreateSpinePointData
CreateSpinePointData(lawValue, parameter, parent)
CreateSpinePointData(lawValueExpression, parameter, parent)
-------------------------------------
Creates a SpinePointData object.
Signature
CreateSpinePointData(lawValue, parameter, parent)
Parameters: - lawValue (float) – Law value
- parameter (float) – Parameter on path
- parent (
NXOpen.Section
) – Section Curve on which projected point lies
Returns: SpinePointData Object
Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
-------------------------------------
Creates a SpinePointData object with expression.
Signature
CreateSpinePointData(lawValueExpression, parameter, parent)
Parameters: - lawValueExpression (
NXOpen.Expression
) – Law value exp - parameter (float) – Parameter on path
- parent (
NXOpen.Section
) – Section Curve on which projected point lies
Returns: SpinePointData Object
Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
-------------------------------------