SmartVolumeProfileBuilder Class¶
-
class
NXOpen.GeometricUtilities.
SmartVolumeProfileBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class contains the options for automatically closing the profile to surrounding model geometry.
It is instantiated in section based sweep operators like extrude and revolve.
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CloseProfileRule | Returns or sets the option defines how to extend the open profile to form a proper intersection with the target body. |
OpenProfileSmartVolumeOption | Returns or sets the option for enabling open profile smart volume. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SmartVolumeProfileBuilderCloseProfileRuleType Enumeration | the type of profile closures to be performed |
Property Detail¶
CloseProfileRule¶
-
SmartVolumeProfileBuilder.
CloseProfileRule
¶ Returns or sets the option defines how to extend the open profile to form a proper intersection with the target body.
-------------------------------------
Getter Method
Signature
CloseProfileRule()
Returns: Return type: NXOpen.GeometricUtilities.SmartVolumeProfileBuilderCloseProfileRuleType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CloseProfileRule(closeProfileRule)
Parameters: closeProfileRule ( NXOpen.GeometricUtilities.SmartVolumeProfileBuilderCloseProfileRuleType
) – the close profile rule.New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OpenProfileSmartVolumeOption¶
-
SmartVolumeProfileBuilder.
OpenProfileSmartVolumeOption
¶ Returns or sets the option for enabling open profile smart volume.
When this option is enabled, extends the tool volume along open end points of the profile to find closure with the target body.
-------------------------------------
Getter Method
Signature
OpenProfileSmartVolumeOption()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OpenProfileSmartVolumeOption(openProfileSmartVolumeOption)
Parameters: openProfileSmartVolumeOption (bool) – If true, enable open profile smart volume. New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
SmartVolumeProfileBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.