SmartVolumeProfileBuilderCloseProfileRuleType Enumeration¶
NXOpen.GeometricUtilities.SmartVolumeProfileBuilder.CloseProfileRuleType is an alias for NXOpen.GeometricUtilities.SmartVolumeProfileBuilderCloseProfileRuleType
-
class
NXOpen.GeometricUtilities.
SmartVolumeProfileBuilderCloseProfileRuleType
¶ Bases:
object
the type of profile closures to be performed
Enum Members
- the first complete intersection with the target. “
- “Lci”, ” Extends the open profile to form
- the last complete intersection with the target. “
- “Cci”, ” For subtract boolean operation,
extends the open profile to form the last complete intersection if the profile lies outside the target excluding the coincident portion. Otherwise, use the first complete intersection. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.