OnPathDistancePatternSpacing Class¶
-
class
NXOpen.GeometricUtilities.
OnPathDistancePatternSpacing
¶ Bases:
NXOpen.GeometricUtilities.PatternSpacing
defines the various ways pattern instances can be spaced within the pattern, particularly in the context of the PatternDefinition class.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
NCopies | Returns the number of copies the pattern will generated in this direction |
OnPathPitchDistance | Returns the distance for the spacing of the pattern from one instance to the next. |
OnPathSpanDistance | Returns the distance for the spacing of the pattern for the entire pattern. |
SpaceType | Returns or sets the type of spacing to be used by the pattern |
SpacingsList | Returns the list of spacings (Expression or OnPathDimBuilder) to be used in this direction |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
OnPathPitchDistance¶
-
OnPathDistancePatternSpacing.
OnPathPitchDistance
¶ Returns the distance for the spacing of the pattern from one instance to the next.
-------------------------------------
Getter Method
Signature
OnPathPitchDistance()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX7.5.0.
License requirements: None.
OnPathSpanDistance¶
-
OnPathDistancePatternSpacing.
OnPathSpanDistance
¶ Returns the distance for the spacing of the pattern for the entire pattern.
-------------------------------------
Getter Method
Signature
OnPathSpanDistance()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
OnPathDistancePatternSpacing.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.