PatternSpacing Class¶
-
class
NXOpen.GeometricUtilities.
PatternSpacing
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
defines the various ways pattern instances can be spaced within the pattern, particularly in the context of the PatternDefinition class.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
NCopies | Returns the number of copies the pattern will generated in this direction |
SpaceType | Returns or sets the type of spacing to be used by the pattern |
SpacingsList | Returns the list of spacings (Expression or OnPathDimBuilder) to be used in this direction |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PatternSpacingSpacingType Enumeration | defines the type of spacing instances can have within a pattern. |
Property Detail¶
NCopies¶
-
PatternSpacing.
NCopies
¶ Returns the number of copies the pattern will generated in this direction
-------------------------------------
Getter Method
Signature
NCopies()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
SpaceType¶
-
PatternSpacing.
SpaceType
¶ Returns or sets the type of spacing to be used by the pattern
-------------------------------------
Getter Method
Signature
SpaceType()
Returns: Return type: NXOpen.GeometricUtilities.PatternSpacingSpacingType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpaceType(spaceType)
Parameters: spaceType ( NXOpen.GeometricUtilities.PatternSpacingSpacingType
) –New in version NX7.5.0.
License requirements: None.
SpacingsList¶
-
PatternSpacing.
SpacingsList
¶ Returns the list of spacings (Expression or OnPathDimBuilder) to be used in this direction
-------------------------------------
Getter Method
Signature
SpacingsList()
Returns: Return type: NXOpen.GeometricUtilities.PatternSpacingsList
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PatternSpacing.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.