Limits Class¶
-
class
NXOpen.GeometricUtilities.
Limits
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a limits data.
New in version NX3.0.1.
Properties¶
Property | Description |
---|---|
EndExtend | Returns the end extend builder |
StartExtend | Returns the start extend builder |
SymmetricOption | Returns or sets the symmetric option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndExtend¶
-
Limits.
EndExtend
¶ Returns the end extend builder
-------------------------------------
Getter Method
Signature
EndExtend()
Returns: Extend object at the end Return type: NXOpen.GeometricUtilities.Extend
New in version NX3.0.1.
License requirements: None.
StartExtend¶
-
Limits.
StartExtend
¶ Returns the start extend builder
-------------------------------------
Getter Method
Signature
StartExtend()
Returns: Extend object at the start Return type: NXOpen.GeometricUtilities.Extend
New in version NX3.0.1.
License requirements: None.
SymmetricOption¶
-
Limits.
SymmetricOption
¶ Returns or sets the symmetric option
-------------------------------------
Getter Method
Signature
SymmetricOption()
Returns: Return type: bool New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
SymmetricOption(symmetricOption)
Parameters: symmetricOption (bool) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
Limits.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.