Extend Class¶
-
class
NXOpen.GeometricUtilities.
Extend
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents an extend data.
New in version NX3.0.1.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Target | Returns or sets the extend target for the following types NXOpen.GeometricUtilities.ExtendExtendType.UntilSelected . |
TrimType | Returns or sets the extend type NXOpen.GeometricUtilities.ExtendExtendType . |
Value | Returns the extend value for the following type NXOpen.GeometricUtilities.ExtendExtendType.Value . |
Methods¶
Method | Description |
---|---|
SetValue | Set extend value for the following type NXOpen.GeometricUtilities.ExtendExtendType.Value . |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExtendExtendType Enumeration | This enum represents the type of extend |
Property Detail¶
Target¶
-
Extend.
Target
¶ Returns or sets the extend target for the following types
NXOpen.GeometricUtilities.ExtendExtendType.UntilSelected
.NXOpen.GeometricUtilities.ExtendExtendType.UntilExtended
.NXOpen.GeometricUtilities.ExtendExtendType.UntilNext
.-------------------------------------
Getter Method
Signature
Target()
Returns: For NXOpen.GeometricUtilities.ExtendExtendType.UntilSelected
it can be face, solid body,sheet body and datums. :rtype:
NXOpen.DisplayableObject
New in version NX3.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Target(selectedObject)
Parameters: selectedObject ( NXOpen.DisplayableObject
) – ForNXOpen.GeometricUtilities.ExtendExtendType.UntilSelected
it can be face, solid body,sheet body and datums.New in version NX3.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
TrimType¶
-
Extend.
TrimType
¶ Returns or sets the extend type
NXOpen.GeometricUtilities.ExtendExtendType
.-------------------------------------
Getter Method
Signature
TrimType()
Returns: Return type: NXOpen.GeometricUtilities.ExtendExtendType
New in version NX3.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimType(extendType)
Parameters: extendType ( NXOpen.GeometricUtilities.ExtendExtendType
) –New in version NX3.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Value¶
-
Extend.
Value
¶ Returns the extend value for the following type
NXOpen.GeometricUtilities.ExtendExtendType.Value
.-------------------------------------
Getter Method
Signature
Value()
Returns: For NXOpen.GeometricUtilities.ExtendExtendType.Value
Return type: NXOpen.Expression
New in version NX3.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
SetValue¶
-
Extend.
SetValue
¶ Set extend value for the following type
NXOpen.GeometricUtilities.ExtendExtendType.Value
.Signature
SetValue(valueExpression)
Parameters: valueExpression (str) – For NXOpen.GeometricUtilities.ExtendExtendType.Value
NOTE: The full Unicode character set is not supported for this parameter.New in version NX3.0.1.
Deprecated since version NX8.5.0: To set the value of the expression modify the expression directly using
GeometricUtilities.Extend.Value
andExpression.RightHandSide
.License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
Extend.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.