FaceSetOffsetCollection Class¶
-
class
NXOpen.GeometricUtilities.
FaceSetOffsetCollection
¶ Bases:
object
This class contains the factory methods for creating an face set offset.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateEmptyFaceSet | Creates an empty offset face set, with all parameters set to 0 or None @return Resultant offset face set |
CreateFaceSet | Creates an offset face set. |
Method Detail¶
CreateEmptyFaceSet¶
-
FaceSetOffsetCollection.
CreateEmptyFaceSet
¶ Creates an empty offset face set, with all parameters set to 0 or None
Signature
CreateEmptyFaceSet()
Returns: Resultant offset face set Return type: NXOpen.GeometricUtilities.FaceSetOffset
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateFaceSet¶
-
FaceSetOffsetCollection.
CreateFaceSet
¶ Creates an offset face set.
Signature
CreateFaceSet(offset, faceCollector, flipValue, index)
Parameters: - offset (str) – Initial expression string for offset distance
- faceCollector (
NXOpen.ScCollector
) – Smart collector for the face set - flipValue (bool) – Whether the faceset should be flipped or not
- index (int) – Index of face set in the list
Returns: Resultant offset face set
Return type: New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)