FaceSetDataCollection Class¶
-
class
NXOpen.GeometricUtilities.
FaceSetDataCollection
¶ Bases:
object
This class contains the factory methods for creating an FaceSetData.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX5.0.0.
Deprecated since version NX8.5.0: This class is never used and can be safely removed
Method Detail¶
Create¶
-
FaceSetDataCollection.
Create
¶ Creates an FaceSetData.
Signature
Create(mFaceCollector, mReverseNormalFlag)
Parameters: - mFaceCollector (
NXOpen.ScCollector
) – the face set collector - mReverseNormalFlag (bool) – the face set reverse direction flag
Returns: Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- mFaceCollector (