BoundingObjectBuilder Class¶
-
class
NXOpen.GeometricUtilities.
BoundingObjectBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.BoundingObjectBuilder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
BoundingCurve | Returns the existing bounding curve. |
BoundingObjectMethod | Returns or sets the bounding object method |
BoundingPlane | Returns or sets the bounding plane. |
BoundingPoint | Returns or sets the bounding point. |
BoundingPoint1 | Returns or sets the bounding point1. |
BoundingPoint2 | Returns or sets the bounding point2. |
BoundingProjectPoint | Returns or sets the bounding project point. |
BoundingVector | Returns or sets the bounding vector. |
IntersectionReference | Returns or sets the intersection reference |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BoundingObjectBuilderMethod Enumeration | Represents Bounding Object option types. |
Property Detail¶
BoundingCurve¶
-
BoundingObjectBuilder.
BoundingCurve
¶ Returns the existing bounding curve.
This is applicable for :py:class:` NXOpen.GeometricUtilities.BoundingObjectBuilderMethod.ExistingCurve < NXOpen.GeometricUtilities.BoundingObjectBuilderMethod>`
-------------------------------------
Getter Method
Signature
BoundingCurve()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX7.5.1.
License requirements: None.
BoundingObjectMethod¶
-
BoundingObjectBuilder.
BoundingObjectMethod
¶ Returns or sets the bounding object method
-------------------------------------
Getter Method
Signature
BoundingObjectMethod()
Returns: Return type: NXOpen.GeometricUtilities.BoundingObjectBuilderMethod
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundingObjectMethod(boundingObjectMethod)
Parameters: boundingObjectMethod ( NXOpen.GeometricUtilities.BoundingObjectBuilderMethod
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
BoundingPlane¶
-
BoundingObjectBuilder.
BoundingPlane
¶ Returns or sets the bounding plane.
This is applicable for :py:class:` NXOpen.GeometricUtilities.BoundingObjectBuilderMethod.ByPlane < NXOpen.GeometricUtilities.BoundingObjectBuilderMethod>`
-------------------------------------
Getter Method
Signature
BoundingPlane()
Returns: Return type: NXOpen.Plane
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundingPlane(plane)
Parameters: plane ( NXOpen.Plane
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
BoundingPoint¶
-
BoundingObjectBuilder.
BoundingPoint
¶ Returns or sets the bounding point.
This is applicable for :py:class:` NXOpen.GeometricUtilities.BoundingObjectBuilderMethod.PointAndVector < NXOpen.GeometricUtilities.BoundingObjectBuilderMethod>`
-------------------------------------
Getter Method
Signature
BoundingPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundingPoint(point)
Parameters: point ( NXOpen.Point
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
BoundingPoint1¶
-
BoundingObjectBuilder.
BoundingPoint1
¶ Returns or sets the bounding point1.
This represents first bounding point. This is applicable for :py:class:` NXOpen.GeometricUtilities.BoundingObjectBuilderMethod.LineBy2Points < NXOpen.GeometricUtilities.BoundingObjectBuilderMethod>`
-------------------------------------
Getter Method
Signature
BoundingPoint1()
Returns: Return type: NXOpen.Point
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundingPoint1(point1)
Parameters: point1 ( NXOpen.Point
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
BoundingPoint2¶
-
BoundingObjectBuilder.
BoundingPoint2
¶ Returns or sets the bounding point2.
This represents second bounding point. This is applicable for :py:class:` NXOpen.GeometricUtilities.BoundingObjectBuilderMethod.LineBy2Points < NXOpen.GeometricUtilities.BoundingObjectBuilderMethod>`
-------------------------------------
Getter Method
Signature
BoundingPoint2()
Returns: Return type: NXOpen.Point
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundingPoint2(point2)
Parameters: point2 ( NXOpen.Point
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
BoundingProjectPoint¶
-
BoundingObjectBuilder.
BoundingProjectPoint
¶ Returns or sets the bounding project point.
This is applicable for :py:class:` NXOpen.GeometricUtilities.BoundingObjectBuilderMethod.ProjectPoint < NXOpen.GeometricUtilities.BoundingObjectBuilderMethod>`
-------------------------------------
Getter Method
Signature
BoundingProjectPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundingProjectPoint(projectPoint)
Parameters: projectPoint ( NXOpen.Point
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
BoundingVector¶
-
BoundingObjectBuilder.
BoundingVector
¶ Returns or sets the bounding vector.
This is applicable for :py:class:` NXOpen.GeometricUtilities.BoundingObjectBuilderMethod.PointAndVector < NXOpen.GeometricUtilities.BoundingObjectBuilderMethod>`
-------------------------------------
Getter Method
Signature
BoundingVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundingVector(vector)
Parameters: vector ( NXOpen.Direction
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
IntersectionReference¶
-
BoundingObjectBuilder.
IntersectionReference
¶ Returns or sets the intersection reference
-------------------------------------
Getter Method
Signature
IntersectionReference()
Returns: Return type: NXOpen.Point
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntersectionReference(intersectionReference)
Parameters: intersectionReference ( NXOpen.Point
) –New in version NX7.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
BoundingObjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.