BlendStopshortBuilderCollection Class¶
-
class
NXOpen.GeometricUtilities.
BlendStopshortBuilderCollection
¶ Bases:
object
This class contains the factory methods for creating an BlendStopshortBuilder.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX5.0.0.
Method Detail¶
Create¶
-
BlendStopshortBuilderCollection.
Create
¶ Creates an BlendStopshortBuilder.
Signature
Create(mChoice, mOnPathExp, mPath, mIsFlipped, mThruPoint)
Parameters: - mChoice (
NXOpen.GeometricUtilities.BlendStopshortBuilderChoices
) – the Stopshort option choice - mOnPathExp (
NXOpen.Expression
) – the expression for the OnPathDimensionBuilder - mPath (
NXOpen.Edge
) – the path for the OnPathDimensionBuilder - mIsFlipped (bool) – the isFlipped flag for the OnPathDimensionBuilder
- mThruPoint (
NXOpen.Point
) – the through point for the OnPathDimensionBuilder
Returns: Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- mChoice (