AngularLimits Class¶
-
class
NXOpen.GeometricUtilities.
AngularLimits
¶ Bases:
NXOpen.GeometricUtilities.Limits
Represents a angular limts data.
New in version NX3.0.1.
Properties¶
Property | Description |
---|---|
Distance | Returns a computed distance |
EndExtend | Returns the end extend builder |
StartExtend | Returns the start extend builder |
SymmetricOption | Returns or sets the symmetric option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Method Detail¶
Validate¶
-
AngularLimits.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.