SurfaceContinuityAnalysisBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
SurfaceContinuityAnalysisBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricAnalysis.SurfaceContinuityAnalysis
builderTo create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisObjectCollection.CreateSurfaceContinuityAnalysisBuilder
Default values.
Property Value CurvatureCheck Sectional G0 True G1 False G2 False G3 False New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CombOptions | Returns the comb display block options |
CurvatureCheck | Returns or sets the curvature check |
Face | Returns the (second) faces. |
FirstEdge | Returns the first edges or faces |
G0 | Returns or sets the g0 toggle |
G1 | Returns or sets the g1 toggle |
G2 | Returns or sets the g2 toggle |
G3 | Returns or sets the g3 toggle |
SecondEdge | Returns the second edges or faces. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of analysis to perform |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFace1Array | Returns the edge1 array not used @return |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateFace | User selects or deselects face, update builder m_edge2, m_face2 |
UpdateFirstEdgeFace | The user selects or deselects first edge or face, update builder m_edge1, m_face1 |
UpdateSecondEdgeFace | User selects or deselects second edge or face, update builder m_edge2, m_face2 |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SurfaceContinuityAnalysisBuilderCurvatureType Enumeration | Curvature types |
SurfaceContinuityAnalysisBuilderTypes Enumeration | Two possible types for the dialog |
Property Detail¶
CombOptions¶
-
SurfaceContinuityAnalysisBuilder.
CombOptions
¶ Returns the comb display block options
-------------------------------------
Getter Method
Signature
CombOptions()
Returns: Return type: NXOpen.GeometricUtilities.CombOptionsBuilder
New in version NX6.0.0.
License requirements: None.
CurvatureCheck¶
-
SurfaceContinuityAnalysisBuilder.
CurvatureCheck
¶ Returns or sets the curvature check
-------------------------------------
Getter Method
Signature
CurvatureCheck()
Returns: Return type: NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderCurvatureType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurvatureCheck(curvatureCheck)
Parameters: curvatureCheck ( NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderCurvatureType
) –New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
Face¶
-
SurfaceContinuityAnalysisBuilder.
Face
¶ Returns the (second) faces.
Used only if the type is EdgeFace
-------------------------------------
Getter Method
Signature
Face()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
FirstEdge¶
-
SurfaceContinuityAnalysisBuilder.
FirstEdge
¶ Returns the first edges or faces
-------------------------------------
Getter Method
Signature
FirstEdge()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
G0¶
-
SurfaceContinuityAnalysisBuilder.
G0
¶ Returns or sets the g0 toggle
-------------------------------------
Getter Method
Signature
G0()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G0(g0)
Parameters: g0 (bool) – New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
G1¶
-
SurfaceContinuityAnalysisBuilder.
G1
¶ Returns or sets the g1 toggle
-------------------------------------
Getter Method
Signature
G1()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G1(g1)
Parameters: g1 (bool) – New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
G2¶
-
SurfaceContinuityAnalysisBuilder.
G2
¶ Returns or sets the g2 toggle
-------------------------------------
Getter Method
Signature
G2()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G2(g2)
Parameters: g2 (bool) – New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
G3¶
-
SurfaceContinuityAnalysisBuilder.
G3
¶ Returns or sets the g3 toggle
-------------------------------------
Getter Method
Signature
G3()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G3(g3)
Parameters: g3 (bool) – New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
SecondEdge¶
-
SurfaceContinuityAnalysisBuilder.
SecondEdge
¶ Returns the second edges or faces.
Used only if the type is EdgeEdge
-------------------------------------
Getter Method
Signature
SecondEdge()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
Type¶
-
SurfaceContinuityAnalysisBuilder.
Type
¶ Returns or sets the type of analysis to perform
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderTypes
) –New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
Method Detail¶
GetFace1Array¶
-
SurfaceContinuityAnalysisBuilder.
GetFace1Array
¶ Returns the edge1 array not used
Signature
GetFace1Array()
Returns: Return type: list of NXOpen.Face
New in version NX6.0.0.
License requirements: None.
UpdateFace¶
-
SurfaceContinuityAnalysisBuilder.
UpdateFace
¶ User selects or deselects face, update builder m_edge2, m_face2
Signature
UpdateFace(face, selectionPoint)
Parameters: - face (
NXOpen.Face
) – - selectionPoint (
NXOpen.Point3d
) –
New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
- face (
UpdateFirstEdgeFace¶
-
SurfaceContinuityAnalysisBuilder.
UpdateFirstEdgeFace
¶ The user selects or deselects first edge or face, update builder m_edge1, m_face1
Signature
UpdateFirstEdgeFace(edgeOrFace, selectionPoint)
Parameters: - edgeOrFace (
NXOpen.DisplayableObject
) – the parent of Face or Edge - selectionPoint (
NXOpen.Point3d
) –
New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
- edgeOrFace (
UpdateSecondEdgeFace¶
-
SurfaceContinuityAnalysisBuilder.
UpdateSecondEdgeFace
¶ User selects or deselects second edge or face, update builder m_edge2, m_face2
Signature
UpdateSecondEdgeFace(edgeOrFace, selectionPoint)
Parameters: - edgeOrFace (
NXOpen.DisplayableObject
) – the parent of Face or Edge - selectionPoint (
NXOpen.Point3d
) –
New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
- edgeOrFace (
Validate¶
-
SurfaceContinuityAnalysisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.