SimpleInterferenceResult Enumeration¶
NXOpen.GeometricAnalysis.SimpleInterference.Result is an alias for NXOpen.GeometricAnalysis.SimpleInterferenceResult
-
class
NXOpen.GeometricAnalysis.
SimpleInterferenceResult
¶ Bases:
object
Specifies the result of a simple interference check
Enum Members
- exists between the input bodies. “
- “OnlyEdgesOrFacesInterfere”, “
Only faces or edges interfere and no solid interference exists between the input bodies. “
“InterferenceExists”, ” Interferenceexists between the input bodies. Use
NXOpen.GeometricAnalysis.SimpleInterference.GetInterferenceResults
to obtain the pairs of faces interfering or interference solid(s) created between the input bodies. ““CanNotPerformCheck”, ” An unknownerror has occured while performing the interference check. Check could not be performed between the input bodies.”
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.