SimpleInterference Class¶
-
class
NXOpen.GeometricAnalysis.
SimpleInterference
¶ Bases:
NXOpen.Builder
Represents the Simple Interference object.
A
NXOpen.GeometricAnalysis.SimpleInterference
object takes two solid bodies as inputs and the type of interference results to be produced. It can report the first pair of interfering faces between two solids or all pairs of interfering faces. It can also create the interference solid(s) between two bodies.To create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisManager.CreateSimpleInterferenceObject
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
FaceInterferenceType | Returns or sets the FaceInterferenceType. |
FirstBody | Returns the First Body |
InterferenceType | Returns or sets the InterferenceType. |
SecondBody | Returns the Second Body |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetInterferenceResults | Returns the pair(s) of interfering faces or solid(s) of interference between the input bodies. |
GetObject | Returns the object currently being edited by this builder. |
HighlightNextPair | Highlights the pairs of interfering faces after a NXOpen.GeometricAnalysis.SimpleInterference.PerformCheck . |
PerformCheck | Perform Interference Check. |
Reset | Frees up resources/results associated with NXOpen.GeometricAnalysis.SimpleInterference object after a call to NXOpen.GeometricAnalysis.SimpleInterference.PerformCheck . |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SimpleInterferenceFaceInterferenceMethod Enumeration | Specifies to find only first pair of interfering faces or all pairs of interfering faces between the input boides. |
SimpleInterferenceInterferenceMethod Enumeration | Specifies interference method, i. |
SimpleInterferenceResult Enumeration | Specifies the result of a simple interference check |
Property Detail¶
FaceInterferenceType¶
-
SimpleInterference.
FaceInterferenceType
¶ Returns or sets the FaceInterferenceType.
NXOpen.GeometricAnalysis.SimpleInterference.FaceInterferenceType`
is used whenNXOpen.GeometricAnalysis.SimpleInterference.InterferenceType`
is set toNXOpen.GeometricAnalysis.SimpleInterferenceInterferenceMethod.InterferingFaces
, i.e., create pair(s) of interfering faces between two solids. A value ofNXOpen.GeometricAnalysis.SimpleInterferenceFaceInterferenceMethod.FirstPairOnly
forNXOpen.GeometricAnalysis.SimpleInterference.FaceInterferenceType`
reports only the first pair of interfering faces and value ofNXOpen.GeometricAnalysis.SimpleInterferenceFaceInterferenceMethod.AllPairs
reports all pairs of interfering faces between two bodies.-------------------------------------
Getter Method
Signature
FaceInterferenceType()
Returns: Return type: NXOpen.GeometricAnalysis.SimpleInterferenceFaceInterferenceMethod
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceInterferenceType(faceInterferenceType)
Parameters: faceInterferenceType ( NXOpen.GeometricAnalysis.SimpleInterferenceFaceInterferenceMethod
) –New in version NX5.0.0.
License requirements: None.
FirstBody¶
-
SimpleInterference.
FirstBody
¶ Returns the First Body
-------------------------------------
Getter Method
Signature
FirstBody()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
InterferenceType¶
-
SimpleInterference.
InterferenceType
¶ Returns or sets the InterferenceType.
A value of
NXOpen.GeometricAnalysis.SimpleInterferenceInterferenceMethod.InterferingFaces
forNXOpen.GeometricAnalysis.SimpleInterference.InterferenceType`
reports the pairs of interfering faces between two solids. You can also further specify to report only the first pair of interfering faces or all pairs of interfering faces byNXOpen.GeometricAnalysis.SimpleInterference.FaceInterferenceType`
. A value ofNXOpen.GeometricAnalysis.SimpleInterferenceInterferenceMethod.InterferenceSolid
forNXOpen.GeometricAnalysis.SimpleInterference.InterferenceType`
creates the interference solid(s) between the two input bodies.-------------------------------------
Getter Method
Signature
InterferenceType()
Returns: Return type: NXOpen.GeometricAnalysis.SimpleInterferenceInterferenceMethod
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterferenceType(interferenceType)
Parameters: interferenceType ( NXOpen.GeometricAnalysis.SimpleInterferenceInterferenceMethod
) –New in version NX5.0.0.
License requirements: None.
SecondBody¶
-
SimpleInterference.
SecondBody
¶ Returns the Second Body
-------------------------------------
Getter Method
Signature
SecondBody()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
Method Detail¶
GetInterferenceResults¶
-
SimpleInterference.
GetInterferenceResults
¶ Returns the pair(s) of interfering faces or solid(s) of interference between the input bodies.
nObjects will be 0 if there is no face or solid interference between the input bodies. If the
NXOpen.GeometricAnalysis.SimpleInterference.InterferenceType`
isNXOpen.GeometricAnalysis.SimpleInterferenceInterferenceMethod.InterferingFaces
, pair(s) of interfering faces are returned. The first two objects represent the first pair of interfering faces, and next two objects represent the second pair of interering faces and so on. If theNXOpen.GeometricAnalysis.SimpleInterference.FaceInterferenceType`
isNXOpen.GeometricAnalysis.SimpleInterferenceFaceInterferenceMethod.FirstPairOnly
, only the first pair of interfering faces are returned.Signature
GetInterferenceResults()
Returns: Results of Simple Interference Return type: list of NXOpen.NXObject
New in version NX6.0.2.
License requirements: None.
HighlightNextPair¶
-
SimpleInterference.
HighlightNextPair
¶ Highlights the pairs of interfering faces after a
NXOpen.GeometricAnalysis.SimpleInterference.PerformCheck
.This method is applicable only when
NXOpen.GeometricAnalysis.SimpleInterference.InterferenceType`
is set toNXOpen.GeometricAnalysis.SimpleInterferenceInterferenceMethod.InterferingFaces
andNXOpen.GeometricAnalysis.SimpleInterference.FaceInterferenceType`
is set toNXOpen.GeometricAnalysis.SimpleInterferenceFaceInterferenceMethod.AllPairs
. When highlighting the next pair, current pair of faces is unhighlighted. Return value is set to true if there are more pairs of faces to be highlighted. If the last pair is reached (i.e., the pair being highlighted in this call is the last pair of faces), return value is set to false.Signature
HighlightNextPair()
Returns: Indicates if there are any more pairs left . :rtype: bool
New in version NX5.0.0.
License requirements: None.
PerformCheck¶
-
SimpleInterference.
PerformCheck
¶ Perform Interference Check.
NXOpen.GeometricAnalysis.SimpleInterference.PerformCheck
should be called after specifiying input bodies to be checked, i.e.,NXOpen.GeometricAnalysis.SimpleInterference.FirstBody
andNXOpen.GeometricAnalysis.SimpleInterference.SecondBody
. The return valueNXOpen.GeometricAnalysis.SimpleInterferenceResult
specifies the type of interference existing between the input bodies. UseNXOpen.GeometricAnalysis.SimpleInterference.GetInterferenceResults
to obtain the interfering faces or solid(s) of interference between the input bodis.Signature
PerformCheck()
Returns: Indicates the type of interference existing between the input bodies. :rtype:
NXOpen.GeometricAnalysis.SimpleInterferenceResult
New in version NX5.0.0.
License requirements: None.
Reset¶
-
SimpleInterference.
Reset
¶ Frees up resources/results associated with
NXOpen.GeometricAnalysis.SimpleInterference
object after a call toNXOpen.GeometricAnalysis.SimpleInterference.PerformCheck
.NXOpen.GeometricAnalysis.SimpleInterference.PerformCheck
is followed byNXOpen.GeometricAnalysis.SimpleInterference.GetInterferenceResults
and theNXOpen.GeometricAnalysis.SimpleInterference.Reset
.Signature
Reset()
New in version NX5.0.0.
License requirements: None.
Validate¶
-
SimpleInterference.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.