WavePointBuilder Class¶
-
class
NXOpen.Features.
WavePointBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
Features.Feature
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateWavePointBuilder
Default values.
Property Value Associative True DrawLineBetweenPoints False InheritDisplayProperties False ParentPart OtherPart New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative |
DrawLineBetweenPoints | Returns or sets the draw line |
FixAtCurrentTimestamp | Returns or sets the fix at timestamp |
FrecAtTimeStamp | Returns or sets the frec at time stamp |
InheritDisplayProperties | Returns or sets the inherit display property option |
MakePositionIndependent | Returns or sets the makepositionindependent |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
ParentPart | Returns or sets the source part type |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Points | Returns the point to link |
SourcePartOccurrence | Returns or sets the source part occurrence |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitCreateOnTheFly | Commits the feature and set create on the fly flag @return |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetProductInterfaceObjects | Gets selected product interface objects |
GetSourcePartOccurrences | Gets source part occurrences |
GetWaveLinkInformation | Prints wave browser type information about link |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetProductInterfaceObjects | Sets selected product interface objects |
SetSourcePartOccurrences | Sets source part occurrences |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WavePointBuilderParentPartType Enumeration | enum for scope of part |
Property Detail¶
Associative¶
-
WavePointBuilder.
Associative
¶ Returns or sets the associative
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
DrawLineBetweenPoints¶
-
WavePointBuilder.
DrawLineBetweenPoints
¶ Returns or sets the draw line
-------------------------------------
Getter Method
Signature
DrawLineBetweenPoints()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawLineBetweenPoints(drawLine)
Parameters: drawLine (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
FixAtCurrentTimestamp¶
-
WavePointBuilder.
FixAtCurrentTimestamp
¶ Returns or sets the fix at timestamp
-------------------------------------
Getter Method
Signature
FixAtCurrentTimestamp()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FixAtCurrentTimestamp(timestamp)
Parameters: timestamp (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
FrecAtTimeStamp¶
-
WavePointBuilder.
FrecAtTimeStamp
¶ Returns or sets the frec at time stamp
-------------------------------------
Getter Method
Signature
FrecAtTimeStamp()
Returns: Return type: NXOpen.Features.Feature
New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrecAtTimeStamp(terminalFrec)
Parameters: terminalFrec ( NXOpen.Features.Feature
) –New in version NX6.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
InheritDisplayProperties¶
-
WavePointBuilder.
InheritDisplayProperties
¶ Returns or sets the inherit display property option
-------------------------------------
Getter Method
Signature
InheritDisplayProperties()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritDisplayProperties(inheritDisplayProperties)
Parameters: inheritDisplayProperties (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
MakePositionIndependent¶
-
WavePointBuilder.
MakePositionIndependent
¶ Returns or sets the makepositionindependent
-------------------------------------
Getter Method
Signature
MakePositionIndependent()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MakePositionIndependent(makePositionIndependent)
Parameters: makePositionIndependent (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
ParentPart¶
-
WavePointBuilder.
ParentPart
¶ Returns or sets the source part type
-------------------------------------
Getter Method
Signature
ParentPart()
Returns: Return type: NXOpen.Features.WavePointBuilderParentPartType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentPart(parentPart)
Parameters: parentPart ( NXOpen.Features.WavePointBuilderParentPartType
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Points¶
-
WavePointBuilder.
Points
¶ Returns the point to link
-------------------------------------
Getter Method
Signature
Points()
Returns: Return type: NXOpen.SelectPointList
New in version NX5.0.0.
License requirements: None.
SourcePartOccurrence¶
-
WavePointBuilder.
SourcePartOccurrence
¶ Returns or sets the source part occurrence
-------------------------------------
Getter Method
Signature
SourcePartOccurrence()
Returns: Return type: NXOpen.TaggedObject
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SourcePartOccurrence(sourcePartOcc)
Parameters: sourcePartOcc ( NXOpen.TaggedObject
) –New in version NX9.0.0.
License requirements: None.
Method Detail¶
CommitCreateOnTheFly¶
-
WavePointBuilder.
CommitCreateOnTheFly
¶ Commits the feature and set create on the fly flag
Signature
CommitCreateOnTheFly()
Returns: Return type: NXOpen.Features.Feature
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
GetProductInterfaceObjects¶
-
WavePointBuilder.
GetProductInterfaceObjects
¶ Gets selected product interface objects
Signature
GetProductInterfaceObjects()
Returns: items in list Return type: list of NXOpen.Assemblies.ProductInterface.InterfaceObject
New in version NX9.0.0.
License requirements: None.
GetSourcePartOccurrences¶
-
WavePointBuilder.
GetSourcePartOccurrences
¶ Gets source part occurrences
Signature
GetSourcePartOccurrences()
Returns: Return type: list of NXOpen.TaggedObject
New in version NX10.0.0.
License requirements: None.
GetWaveLinkInformation¶
-
WavePointBuilder.
GetWaveLinkInformation
¶ Prints wave browser type information about link
Signature
GetWaveLinkInformation()
Returns: a tuple Return type: A tuple consisting of (info, xformExists, xformOrigin, xformOrientation, xformScale). info is a str. queried wave information xformExists is a bool. true if there is a transform xformOrigin is a NXOpen.Point3d
. transformation origin xformOrientation is aNXOpen.Matrix3x3
. transformation matrix xformScale is a float. transformation scaleNew in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
SetProductInterfaceObjects¶
-
WavePointBuilder.
SetProductInterfaceObjects
¶ Sets selected product interface objects
Signature
SetProductInterfaceObjects(selectedObjects)
Parameters: selectedObjects (list of NXOpen.Assemblies.ProductInterface.InterfaceObject
) – items in listNew in version NX9.0.0.
License requirements: None.
SetSourcePartOccurrences¶
-
WavePointBuilder.
SetSourcePartOccurrences
¶ Sets source part occurrences
Signature
SetSourcePartOccurrences(sourcePartOccurrences)
Parameters: sourcePartOccurrences (list of NXOpen.TaggedObject
) –New in version NX10.0.0.
License requirements: None.
Validate¶
-
WavePointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.