CageManipulatorDataObjectMoveData_Struct Struct¶
NXOpen.Features.Subdivision.CageManipulatorData.ObjectMoveData is an alias for NXOpen.Features.Subdivision.CageManipulatorDataObjectMoveData_Struct
-
class
NXOpen.Features.Subdivision.
CageManipulatorDataObjectMoveData_Struct
¶ Bases:
object
Contains object movement information.
New in version NX9.0.0.
Fields¶
Field | Description |
---|---|
DraggedObject | The dragged object. |
BeginDragCursorPosition | The point from which object dragging is initiated, the point under the cursor when seen in view direction. |
BeginDragObjectPosition | The point on object near cursor from which object dragging is initiated |
View | The view in which object is dragged. |
MicropositioningScale | The micropositioning scale. |
ViewDirection | The view direction. |
DraggedObject¶
-
CageManipulatorDataObjectMoveData_Struct.
DraggedObject
¶ The dragged object.
-------------------------------------
Getter Method Signature
DraggedObject()
Returns: Return type: NXOpen.NXObject
-------------------------------------
Setter Method
Signature
DraggedObject(value)
Parameters: value ( NXOpen.NXObject
) –
BeginDragCursorPosition¶
-
CageManipulatorDataObjectMoveData_Struct.
BeginDragCursorPosition
¶ The point from which object dragging is initiated, the point under the cursor when seen in view direction.
-------------------------------------
Getter Method Signature
BeginDragCursorPosition()
Returns: Return type: NXOpen.Point3d
-------------------------------------
Setter Method
Signature
BeginDragCursorPosition(value)
Parameters: value ( NXOpen.Point3d
) –
BeginDragObjectPosition¶
-
CageManipulatorDataObjectMoveData_Struct.
BeginDragObjectPosition
¶ The point on object near cursor from which object dragging is initiated
-------------------------------------
Getter Method Signature
BeginDragObjectPosition()
Returns: Return type: NXOpen.Point3d
-------------------------------------
Setter Method
Signature
BeginDragObjectPosition(value)
Parameters: value ( NXOpen.Point3d
) –
View¶
-
CageManipulatorDataObjectMoveData_Struct.
View
¶ The view in which object is dragged.
-------------------------------------
Getter Method Signature
View()
Returns: Return type: NXOpen.View
-------------------------------------
Setter Method
Signature
View(value)
Parameters: value ( NXOpen.View
) –
MicropositioningScale¶
-
CageManipulatorDataObjectMoveData_Struct.
MicropositioningScale
¶ The micropositioning scale.
-------------------------------------
Getter Method Signature
MicropositioningScale()
Returns: Return type: float -------------------------------------
Setter Method
Signature
MicropositioningScale(value)
Parameters: value (float) –
ViewDirection¶
-
CageManipulatorDataObjectMoveData_Struct.
ViewDirection
¶ The view direction.
-------------------------------------
Getter Method Signature
ViewDirection()
Returns: Return type: NXOpen.Vector3d
-------------------------------------
Setter Method
Signature
ViewDirection(value)
Parameters: value ( NXOpen.Vector3d
) –