SphericalCornerBuilder Class¶
-
class
NXOpen.Features.
SphericalCornerBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.SphericalCorner
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSphericalCornerBuilder
Default values.
Property Value Radius.Value 5 (millimeters part), 0.25 (inches part) New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AngleTol | Returns or sets the Angular Tolerance |
DistanceTol | Returns or sets the Distance Tolerance |
HelpPoint | Returns or sets the Help point acquired from the first face set selection |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Radius | Returns the Radius of the spherical corner |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Wall1 | Returns the wall faces 1 |
Wall2 | Returns the wall faces 2 |
Wall3 | Returns the wall faces 3 |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTol¶
-
SphericalCornerBuilder.
AngleTol
¶ Returns or sets the Angular Tolerance
-------------------------------------
Getter Method
Signature
AngleTol()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTol(angleTol)
Parameters: angleTol (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistanceTol¶
-
SphericalCornerBuilder.
DistanceTol
¶ Returns or sets the Distance Tolerance
-------------------------------------
Getter Method
Signature
DistanceTol()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTol(distanceTol)
Parameters: distanceTol (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
HelpPoint¶
-
SphericalCornerBuilder.
HelpPoint
¶ Returns or sets the Help point acquired from the first face set selection
-------------------------------------
Getter Method
Signature
HelpPoint()
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HelpPoint(helpPoint)
Parameters: helpPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Radius¶
-
SphericalCornerBuilder.
Radius
¶ Returns the Radius of the spherical corner
-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Wall1¶
-
SphericalCornerBuilder.
Wall1
¶ Returns the wall faces 1
-------------------------------------
Getter Method
Signature
Wall1()
Returns: Return type: NXOpen.GeometricUtilities.FaceSetData
New in version NX8.5.0.
License requirements: None.
Wall2¶
-
SphericalCornerBuilder.
Wall2
¶ Returns the wall faces 2
-------------------------------------
Getter Method
Signature
Wall2()
Returns: Return type: NXOpen.GeometricUtilities.FaceSetData
New in version NX8.5.0.
License requirements: None.
Wall3¶
-
SphericalCornerBuilder.
Wall3
¶ Returns the wall faces 3
-------------------------------------
Getter Method
Signature
Wall3()
Returns: Return type: NXOpen.GeometricUtilities.FaceSetData
New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
SphericalCornerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.