SmoothSplineBuilder Class¶
-
class
NXOpen.Features.
SmoothSplineBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.SmoothSpline
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSmoothSplineBuilder
Default values.
Property Value CurveRange.AnchorPosition Start ModificationPercentage 100 SmoothingFactor 1 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Curve | Returns the curve |
CurveRange | Returns the curve range |
EndConstraint | Returns the end constraint |
ModificationPercentage | Returns or sets the modification percentage |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SmoothingFactor | Returns or sets the smoothing factor |
StartConstraint | Returns the start constraint |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SmoothSplineBuilderTypes Enumeration | This enum represents the Smoothing Type option |
Property Detail¶
Curve¶
-
SmoothSplineBuilder.
Curve
¶ Returns the curve
-------------------------------------
Getter Method
Signature
Curve()
Returns: Return type: NXOpen.SelectCurve
New in version NX6.0.0.
License requirements: None.
CurveRange¶
-
SmoothSplineBuilder.
CurveRange
¶ Returns the curve range
-------------------------------------
Getter Method
Signature
CurveRange()
Returns: Return type: NXOpen.GeometricUtilities.CurveRangeBuilder
New in version NX6.0.0.
License requirements: None.
EndConstraint¶
-
SmoothSplineBuilder.
EndConstraint
¶ Returns the end constraint
-------------------------------------
Getter Method
Signature
EndConstraint()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ModificationPercentage¶
-
SmoothSplineBuilder.
ModificationPercentage
¶ Returns or sets the modification percentage
-------------------------------------
Getter Method
Signature
ModificationPercentage()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModificationPercentage(modificationPercentage)
Parameters: modificationPercentage (int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
SmoothingFactor¶
-
SmoothSplineBuilder.
SmoothingFactor
¶ Returns or sets the smoothing factor
-------------------------------------
Getter Method
Signature
SmoothingFactor()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothingFactor(smoothingFactor)
Parameters: smoothingFactor (int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
StartConstraint¶
-
SmoothSplineBuilder.
StartConstraint
¶ Returns the start constraint
-------------------------------------
Getter Method
Signature
StartConstraint()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
Type¶
-
SmoothSplineBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.SmoothSplineBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.SmoothSplineBuilderTypes
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
SmoothSplineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.