Properties¶
Property | Description |
---|---|
OffsetRelations | Returns or sets the value indicating whether to keep offset relations or not |
RelatedFace | Returns the related face |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
DeleteAllConstraints | Deletes all the persistent constraints on the related face |
DeleteAllOffsetRelationOnBody | Deletes all the offset relations on the body which the face belongs to |
DeleteConstraint | Deletes the persistent constraint |
DeleteOffsetRelation | Deletes the offset relation |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
LockConstraint | Locks the persistent constraint |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnlockAllConstraints | Unlocks all the persistent constraints on the related face |
UnlockConstraint | Unlocks the persistent constraint |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
OffsetRelations¶
-
ShowRelatedFacesBuilder.
OffsetRelations
¶ Returns or sets the value indicating whether to keep offset relations or not
-------------------------------------
Getter Method
Signature
OffsetRelations()
Returns: Flag indicating whether to include the offset relation Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetRelations(keepOffsetRelations)
Parameters: keepOffsetRelations (bool) – Flag indicating whether to include the offset relation New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Method Detail¶
DeleteAllConstraints¶
-
ShowRelatedFacesBuilder.
DeleteAllConstraints
¶ Deletes all the persistent constraints on the related face
Signature
DeleteAllConstraints()
New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
DeleteAllOffsetRelationOnBody¶
-
ShowRelatedFacesBuilder.
DeleteAllOffsetRelationOnBody
¶ Deletes all the offset relations on the body which the face belongs to
Signature
DeleteAllOffsetRelationOnBody()
New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
DeleteConstraint¶
-
ShowRelatedFacesBuilder.
DeleteConstraint
¶ Deletes the persistent constraint
Signature
DeleteConstraint(feature)
Parameters: feature ( NXOpen.Features.Feature
) – the persistent constraint featureNew in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
DeleteOffsetRelation¶
-
ShowRelatedFacesBuilder.
DeleteOffsetRelation
¶ Deletes the offset relation
Signature
DeleteOffsetRelation(offsetFaces)
Parameters: offsetFaces (list of NXOpen.NXObject
) –New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
LockConstraint¶
-
ShowRelatedFacesBuilder.
LockConstraint
¶ Locks the persistent constraint
Signature
LockConstraint(feature)
Parameters: feature ( NXOpen.Features.Feature
) – the persistent constraint featureNew in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
UnlockAllConstraints¶
-
ShowRelatedFacesBuilder.
UnlockAllConstraints
¶ Unlocks all the persistent constraints on the related face
Signature
UnlockAllConstraints()
New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
UnlockConstraint¶
-
ShowRelatedFacesBuilder.
UnlockConstraint
¶ Unlocks the persistent constraint
Signature
UnlockConstraint(feature)
Parameters: feature ( NXOpen.Features.Feature
) – the persistent constraint featureNew in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Validate¶
-
ShowRelatedFacesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.