ResizeChamferBuilder Class¶
-
class
NXOpen.Features.
ResizeChamferBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ResizeChamfer
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateResizeChamferBuilder
Default values.
Property Value Angle.Value 0 ChamferType SymmetricOffset Offset1.Value 0 (millimeters part), 0 (inches part) Offset2.Value 0 (millimeters part), 0 (inches part) New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle |
ChamferType | Returns or sets the chamfer type |
Faces | Returns the faces |
FlipChamferOffsets | Returns or sets the flip flag |
Offset1 | Returns the offset1 |
Offset2 | Returns the offset2 |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ResizeChamferBuilderSectionType Enumeration | the chamfer section types |
Property Detail¶
Angle¶
-
ResizeChamferBuilder.
Angle
¶ Returns the angle
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: NXOpen.Expression
New in version NX7.0.0.
License requirements: None.
ChamferType¶
-
ResizeChamferBuilder.
ChamferType
¶ Returns or sets the chamfer type
-------------------------------------
Getter Method
Signature
ChamferType()
Returns: Return type: NXOpen.Features.ResizeChamferBuilderSectionType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChamferType(chamferType)
Parameters: chamferType ( NXOpen.Features.ResizeChamferBuilderSectionType
) –New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Faces¶
-
ResizeChamferBuilder.
Faces
¶ Returns the faces
-------------------------------------
Getter Method
Signature
Faces()
Returns: Return type: NXOpen.ScCollector
New in version NX7.0.0.
License requirements: None.
FlipChamferOffsets¶
-
ResizeChamferBuilder.
FlipChamferOffsets
¶ Returns or sets the flip flag
-------------------------------------
Getter Method
Signature
FlipChamferOffsets()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlipChamferOffsets(flipChamferOffsets)
Parameters: flipChamferOffsets (bool) – New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Offset1¶
-
ResizeChamferBuilder.
Offset1
¶ Returns the offset1
-------------------------------------
Getter Method
Signature
Offset1()
Returns: Return type: NXOpen.Expression
New in version NX7.0.0.
License requirements: None.
Offset2¶
-
ResizeChamferBuilder.
Offset2
¶ Returns the offset2
-------------------------------------
Getter Method
Signature
Offset2()
Returns: Return type: NXOpen.Expression
New in version NX7.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ResizeChamferBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.