ReorderBlendsBuilder Class¶
-
class
NXOpen.Features.
ReorderBlendsBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ReorderBlends
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateReorderBlendsBuilder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
BlendFace1 | Returns the blend face1 |
BlendFace2 | Returns the blend face2 |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetBlendface2Candidate | Auto find blend face2 which has overflow to a given blend face(as blend face1). |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BlendFace1¶
-
ReorderBlendsBuilder.
BlendFace1
¶ Returns the blend face1
-------------------------------------
Getter Method
Signature
BlendFace1()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.1.
License requirements: None.
BlendFace2¶
-
ReorderBlendsBuilder.
BlendFace2
¶ Returns the blend face2
-------------------------------------
Getter Method
Signature
BlendFace2()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.1.
License requirements: None.
Method Detail¶
GetBlendface2Candidate¶
-
ReorderBlendsBuilder.
GetBlendface2Candidate
¶ Auto find blend face2 which has overflow to a given blend face(as blend face1).
Return cases: Output/return vary based on number of candidate found:
when 0 candidate found -<ja_gt> blendFace2 = None error = DMX_REORDER_BLEND_NO_INTERACTION
when 1 candidate found -<ja_gt> blendFace2 = candidate, error = CM_NO_ERRORS
when <ja_gt>1 candidates found -<ja_gt> blendFace2 = None, error = CM_NO_ERRORS;
Signature
GetBlendface2Candidate(blendFace1)
Parameters: blendFace1 ( NXOpen.Face
) – A blend face for finding its overflow blend faceReturns: A blend face which has overflow with blendFace1 Return type: NXOpen.Face
New in version NX7.5.1.
License requirements: None.
Validate¶
-
ReorderBlendsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.