RefitFaceBuilder Class¶
-
class
NXOpen.Features.
RefitFaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.RefitFace
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateRefitFaceBuilder
Default values.
Property Value RefitControl.DegreesAndSegmentsOrPatches.Degree 3 RefitControl.DegreesAndSegmentsOrPatches.SegmentsOrPatches 1 RefitControl.DegreesAndSegmentsOrPatches.UDegree 5 RefitControl.DegreesAndSegmentsOrPatches.UPatches 1 RefitControl.DegreesAndSegmentsOrPatches.VDegree 5 RefitControl.DegreesAndSegmentsOrPatches.VPatches 1 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ConstraintUMax | Returns the refit face Umax constraint |
ConstraintUMin | Returns the refit face Umin constraint |
ConstraintVMax | Returns the refit face Vmax constraint |
ConstraintVMin | Returns the refit face Vmin constraint |
Face | Returns the refitting face |
FitDirection | Returns or sets the refit face fit direction |
HasFitDirection | Returns or sets a flag that shows refit face direction in use |
IsCreateCopy | Returns or sets the new copy of match edge surface |
MaxCheckingDist | Returns or sets the refit face max check distance |
ModificationPercent | Returns or sets the refit face modification percentage |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RefitControl | Returns the refit control parameters - type, degree, patches, direction, tolerance |
SmoothFactor | Returns or sets the refit face smoothing factor |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Targets | Returns the list of targets |
Type | Returns or sets the refit type |
UseConstraintsAll | Returns or sets the refit face constraints use flag |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RefitFaceBuilderTypes Enumeration | the type of face refit |
Property Detail¶
ConstraintUMax¶
-
RefitFaceBuilder.
ConstraintUMax
¶ Returns the refit face Umax constraint
-------------------------------------
Getter Method
Signature
ConstraintUMax()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ConstraintUMin¶
-
RefitFaceBuilder.
ConstraintUMin
¶ Returns the refit face Umin constraint
-------------------------------------
Getter Method
Signature
ConstraintUMin()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ConstraintVMax¶
-
RefitFaceBuilder.
ConstraintVMax
¶ Returns the refit face Vmax constraint
-------------------------------------
Getter Method
Signature
ConstraintVMax()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ConstraintVMin¶
-
RefitFaceBuilder.
ConstraintVMin
¶ Returns the refit face Vmin constraint
-------------------------------------
Getter Method
Signature
ConstraintVMin()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
Face¶
-
RefitFaceBuilder.
Face
¶ Returns the refitting face
-------------------------------------
Getter Method
Signature
Face()
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX6.0.0.
License requirements: None.
FitDirection¶
-
RefitFaceBuilder.
FitDirection
¶ Returns or sets the refit face fit direction
-------------------------------------
Getter Method
Signature
FitDirection()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FitDirection(fitDir)
Parameters: fitDir ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
HasFitDirection¶
-
RefitFaceBuilder.
HasFitDirection
¶ Returns or sets a flag that shows refit face direction in use
-------------------------------------
Getter Method
Signature
HasFitDirection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HasFitDirection(hasFitDir)
Parameters: hasFitDir (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsCreateCopy¶
-
RefitFaceBuilder.
IsCreateCopy
¶ Returns or sets the new copy of match edge surface
-------------------------------------
Getter Method
Signature
IsCreateCopy()
Returns: Return type: bool New in version NX6.0.1.
License requirements: features_modeling (“FEATURES MODELING”)
-------------------------------------
Setter Method
Signature
IsCreateCopy(createCopy)
Parameters: createCopy (bool) – New in version NX6.0.1.
License requirements: features_modeling (“FEATURES MODELING”)
MaxCheckingDist¶
-
RefitFaceBuilder.
MaxCheckingDist
¶ Returns or sets the refit face max check distance
-------------------------------------
Getter Method
Signature
MaxCheckingDist()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxCheckingDist(maxChckDst)
Parameters: maxChckDst (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ModificationPercent¶
-
RefitFaceBuilder.
ModificationPercent
¶ Returns or sets the refit face modification percentage
-------------------------------------
Getter Method
Signature
ModificationPercent()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModificationPercent(modPercent)
Parameters: modPercent (int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RefitControl¶
-
RefitFaceBuilder.
RefitControl
¶ Returns the refit control parameters - type, degree, patches, direction, tolerance
-------------------------------------
Getter Method
Signature
RefitControl()
Returns: Return type: NXOpen.GeometricUtilities.RefitControlBuilder
New in version NX6.0.0.
License requirements: None.
SmoothFactor¶
-
RefitFaceBuilder.
SmoothFactor
¶ Returns or sets the refit face smoothing factor
-------------------------------------
Getter Method
Signature
SmoothFactor()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothFactor(refitFaceSmoothFac)
Parameters: refitFaceSmoothFac (int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Targets¶
-
RefitFaceBuilder.
Targets
¶ Returns the list of targets
-------------------------------------
Getter Method
Signature
Targets()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX6.0.0.
License requirements: None.
Type¶
-
RefitFaceBuilder.
Type
¶ Returns or sets the refit type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.RefitFaceBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.RefitFaceBuilderTypes
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UseConstraintsAll¶
-
RefitFaceBuilder.
UseConstraintsAll
¶ Returns or sets the refit face constraints use flag
-------------------------------------
Getter Method
Signature
UseConstraintsAll()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseConstraintsAll(constrAll)
Parameters: constrAll (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
RefitFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.