ReferenceMapperBuilder Class¶
-
class
NXOpen.Features.
ReferenceMapperBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.ReferenceMapperBuilder
It is used in the context of Boolean Target/Tool Mapping.Mapping needs to be done when the user edits a Boolean feature and adds/removes tools and/or target.The ReferenceMapper populates
NXOpen.Features.FeatureReferencesBuilder
with the references of the removed tools and/or target and gives the user an opportunity to map it with the references of the newly added tools and/or target.To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateReferenceMapperBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
FeatureReferences | Returns the Feature References Builder |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FeatureReferences¶
-
ReferenceMapperBuilder.
FeatureReferences
¶ Returns the Feature References Builder
-------------------------------------
Getter Method
Signature
FeatureReferences()
Returns: Return type: NXOpen.Features.FeatureReferencesBuilder
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
ReferenceMapperBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.