PatternFeatureBuilder Class¶
-
class
NXOpen.Features.
PatternFeatureBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.PatternFeature
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreatePatternFeatureBuilder
Default values.
Property Value CreateReferencePattern True ExpressionOption CreateNew OutputOption PatternFeature PatternMethod Variational PatternService.AlongPathDefinition.XOnPathSpacing.NCopies.Value 2 PatternService.AlongPathDefinition.XOnPathSpacing.SpaceType Offset PatternService.AlongPathDefinition.XPathOption Offset PatternService.AlongPathDefinition.YDirectionOption Section PatternService.AlongPathDefinition.YOnPathSpacing.NCopies.Value 1 PatternService.AlongPathDefinition.YPathOption Offset PatternService.AlongPathDefinition.YSpacing.NCopies.Value 1 PatternService.AlongPathDefinition.YSpacing.PitchDistance.Value 10 (millimeters part), 1 (inches part) PatternService.AlongPathDefinition.YSpacing.SpaceType Offset PatternService.AlongPathDefinition.YSpacing.SpanDistance.Value 100 (millimeters part), 10 (inches part) PatternService.CircularDefinition.AngularSpacing.NCopies.Value 12 PatternService.CircularDefinition.AngularSpacing.PitchAngle.Value 30 PatternService.CircularDefinition.AngularSpacing.PitchDistance.Value 10 (millimeters part), 1 (inches part) PatternService.CircularDefinition.AngularSpacing.SpaceType Offset PatternService.CircularDefinition.AngularSpacing.SpanAngle.Value 360 (millimeters part), 360 (inches part) PatternService.CircularDefinition.AngularSpacing.UsePitchOption Angle PatternService.CircularDefinition.CreateLastStaggered true PatternService.CircularDefinition.HorizontalRef.RotationAngle.Value 0 (millimeters part), 0 (inches part) PatternService.CircularDefinition.IncludeSeedToggle true PatternService.CircularDefinition.RadialSpacing.NCopies.Value 1 PatternService.CircularDefinition.StaggerType None PatternService.HelixDefinition.AnglePitch.Value 30 PatternService.HelixDefinition.CountOfInstances.Value 6 PatternService.HelixDefinition.DirectionType Righthand PatternService.HelixDefinition.DistancePitch.Value 10 (millimeters part), 0.4 (inches part) PatternService.HelixDefinition.HelixPitch.Value 50 (millimeters part), 2 (inches part) PatternService.HelixDefinition.HelixSpan.Value 100 (millimeters part), 4 (inches part) PatternService.HelixDefinition.NumberOfTurns.Value 2 PatternService.HelixDefinition.SizeOption CountAngleDistance PatternService.PatternFill.FillMargin.Value 0 (millimeters part), 0 (inches part) PatternService.PatternFill.FillOptions None PatternService.PatternFill.SimplifiedBoundaryToggle False PatternService.PatternOrientation.AlongOrientationOption NormalToPath PatternService.PatternOrientation.CircularOrientationOption FollowPattern PatternService.PatternOrientation.FollowFaceProjDirOption PatternPlaneNormal PatternService.PatternOrientation.GeneralOrientationOption Fixed PatternService.PatternOrientation.HelixOrientationOption FollowPattern PatternService.PatternOrientation.LinearOrientationOption Fixed PatternService.PatternOrientation.MirrorOrientationOption FollowPattern PatternService.PatternOrientation.OrientationOption Fixed PatternService.PatternOrientation.PolygonOrientationOption FollowPattern PatternService.PatternOrientation.SpiralOrientationOption FollowPattern PatternService.PatternType Linear PatternService.PolygonDefinition.NumberOfSides.Value 6 PatternService.PolygonDefinition.PolygonSizeOption Inscribed PatternService.PolygonDefinition.PolygonSpacing.NCopies.Value 4 PatternService.PolygonDefinition.PolygonSpacing.PitchDistance.Value 25 (millimeters part), 1 (inches part) PatternService.PolygonDefinition.PolygonSpacing.SpaceType Offset PatternService.PolygonDefinition.PolygonSpacing.SpanAngle.Value 360 PatternService.PolygonDefinition.RadialSpacing.NCopies.Value 1 PatternService.PolygonDefinition.RadialSpacing.PitchDistance.Value 25 (millimeters part), 1 (inches part) PatternService.PolygonDefinition.RadialSpacing.SpanDistance.Value 100 (millimeters part), 4 (inches part) PatternService.RectangularDefinition.CreateLastStaggered true PatternService.RectangularDefinition.SimplifiedLayoutType Square PatternService.RectangularDefinition.StaggerType None PatternService.RectangularDefinition.XSpacing.NCopies.Value 2 PatternService.RectangularDefinition.YSpacing.NCopies.Value 1 PatternService.SpiralDefinition.DirectionType Lefthand PatternService.SpiralDefinition.NumberOfTurns.Value 1 (millimeters part), 1 (inches part) PatternService.SpiralDefinition.RadialPitch.Value 50 (millimeters part), 2 (inches part) PatternService.SpiralDefinition.SizeSpiralType NumberOfTurns PatternService.SpiralDefinition.TotalAngle.Value 360 (millimeters part), 360 (inches part) UseInferredReferencePoint (deprecated) True New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
CreateReferencePattern | Returns or sets the Create Reference Pattern option |
ExpressionOption | Returns or sets the expression transfer option |
FeatureList | Returns the Features |
OutputOption | Returns or sets the output option |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PatternMethod | Returns or sets the Pattern method |
PatternService | Returns the Pattern definition service |
ReferencePoint | Returns or sets the reference point |
ReferencePointService | Returns the reference point service |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
UseInferredReferencePoint | Returns or sets a flag to indicate whether to use reference point inferred from selected feature(s) or not. |
Methods¶
Method | Description |
---|---|
ClearReferencesToReuse | Clears all the existing references to reuse so that new references can be added |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
RemoveAllClocking | Removes clocking from (unclocks) all instances of the NXOpen.Features.PatternFeature . |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetReferencesToReuse | Sets the references or selections from the input features which are to be reused for all instances. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PatternFeatureBuilderExpressionTransferOptions Enumeration | the Expression transfer options. |
PatternFeatureBuilderOutputOptions Enumeration | the Output options. |
PatternFeatureBuilderPatternMethodOptions Enumeration | the Pattern method options. |
Property Detail¶
CreateReferencePattern¶
-
PatternFeatureBuilder.
CreateReferencePattern
¶ Returns or sets the Create Reference Pattern option
-------------------------------------
Getter Method
Signature
CreateReferencePattern()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateReferencePattern(createReferencePattern)
Parameters: createReferencePattern (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ExpressionOption¶
-
PatternFeatureBuilder.
ExpressionOption
¶ Returns or sets the expression transfer option
-------------------------------------
Getter Method
Signature
ExpressionOption()
Returns: Return type: NXOpen.Features.PatternFeatureBuilderExpressionTransferOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExpressionOption(expressionOption)
Parameters: expressionOption ( NXOpen.Features.PatternFeatureBuilderExpressionTransferOptions
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FeatureList¶
-
PatternFeatureBuilder.
FeatureList
¶ Returns the Features
-------------------------------------
Getter Method
Signature
FeatureList()
Returns: Return type: NXOpen.Features.SelectFeatureList
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OutputOption¶
-
PatternFeatureBuilder.
OutputOption
¶ Returns or sets the output option
-------------------------------------
Getter Method
Signature
OutputOption()
Returns: Return type: NXOpen.Features.PatternFeatureBuilderOutputOptions
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputOption(outputOption)
Parameters: outputOption ( NXOpen.Features.PatternFeatureBuilderOutputOptions
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PatternMethod¶
-
PatternFeatureBuilder.
PatternMethod
¶ Returns or sets the Pattern method
-------------------------------------
Getter Method
Signature
PatternMethod()
Returns: Return type: NXOpen.Features.PatternFeatureBuilderPatternMethodOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PatternMethod(methodOption)
Parameters: methodOption ( NXOpen.Features.PatternFeatureBuilderPatternMethodOptions
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PatternService¶
-
PatternFeatureBuilder.
PatternService
¶ Returns the Pattern definition service
-------------------------------------
Getter Method
Signature
PatternService()
Returns: Return type: NXOpen.GeometricUtilities.PatternDefinition
New in version NX7.5.0.
License requirements: None.
ReferencePoint¶
-
PatternFeatureBuilder.
ReferencePoint
¶ Returns or sets the reference point
-------------------------------------
Getter Method
Signature
ReferencePoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
GeometricUtilities.PatternReferencePointServiceBuilder.Point
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePoint(referencePoint)
Parameters: referencePoint ( NXOpen.Point
) –New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
GeometricUtilities.PatternReferencePointServiceBuilder.Point
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
ReferencePointService¶
-
PatternFeatureBuilder.
ReferencePointService
¶ Returns the reference point service
-------------------------------------
Getter Method
Signature
ReferencePointService()
Returns: Return type: NXOpen.GeometricUtilities.PatternReferencePointServiceBuilder
New in version NX9.0.0.
License requirements: None.
UseInferredReferencePoint¶
-
PatternFeatureBuilder.
UseInferredReferencePoint
¶ Returns or sets a flag to indicate whether to use reference point inferred from selected feature(s) or not.
If ‘true’, the reference point will be inferred every time the selected feature(s) get modified or updates. If ‘false, the reference point provided will be independent of the selected feature(s) but will be associative to the rule by which it was created (e.g. End of Line, Center of Arc).
-------------------------------------
Getter Method
Signature
UseInferredReferencePoint()
Returns: Return type: bool New in version NX8.0.0.
Deprecated since version NX9.0.0: Use
GeometricUtilities.PatternReferencePointServiceBuilder.IsReferencePointInferred
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
UseInferredReferencePoint(useInferredReferencePoint)
Parameters: useInferredReferencePoint (bool) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Use
GeometricUtilities.PatternReferencePointServiceBuilder.IsReferencePointInferred
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
ClearReferencesToReuse¶
-
PatternFeatureBuilder.
ClearReferencesToReuse
¶ Clears all the existing references to reuse so that new references can be added
Signature
ClearReferencesToReuse()
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveAllClocking¶
-
PatternFeatureBuilder.
RemoveAllClocking
¶ Removes clocking from (unclocks) all instances of the
NXOpen.Features.PatternFeature
.Signature
RemoveAllClocking()
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetReferencesToReuse¶
-
PatternFeatureBuilder.
SetReferencesToReuse
¶ Sets the references or selections from the input features which are to be reused for all instances.
The references for reuse should belong to some input feature which needs to be specified while calling this API.
Signature
SetReferencesToReuse(inputFeature, referencesFromInputFeatures)
Parameters: - inputFeature (
NXOpen.Features.Feature
) – - referencesFromInputFeatures (list of
NXOpen.NXObject
) –
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- inputFeature (
Validate¶
-
PatternFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.