OptimizeFaceBuilder Class¶
-
class
NXOpen.Features.
OptimizeFaceBuilder
¶ Bases:
NXOpen.Builder
Represents a builder of optimize face
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateOptimizeFaceBuilder
Default values.
Property Value CleanBody 1 Report 1 New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
CleanBody | Returns or sets the clean body flag. |
DistanceTolerance | Returns or sets the distance tolerance |
FacesToOptimize | Returns the faces to optimize |
Report | Returns or sets the report flag. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CleanBody¶
-
OptimizeFaceBuilder.
CleanBody
¶ Returns or sets the clean body flag.
If true, cleans body before optimization, else doesn’t.
-------------------------------------
Getter Method
Signature
CleanBody()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CleanBody(cleanBody)
Parameters: cleanBody (bool) – New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
DistanceTolerance¶
-
OptimizeFaceBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
FacesToOptimize¶
-
OptimizeFaceBuilder.
FacesToOptimize
¶ Returns the faces to optimize
-------------------------------------
Getter Method
Signature
FacesToOptimize()
Returns: Return type: NXOpen.ScCollector
New in version NX7.0.0.
License requirements: None.
Report¶
-
OptimizeFaceBuilder.
Report
¶ Returns or sets the report flag.
If true, generates a report of changed faces and edges before and after the face optimization. If false, no report is generated.
-------------------------------------
Getter Method
Signature
Report()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Report(report)
Parameters: report (bool) – New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
OptimizeFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.