OptimizeCurveBuilder Class¶
-
class
NXOpen.Features.
OptimizeCurveBuilder
¶ Bases:
NXOpen.Builder
Represents a builder of optimize curve
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateOptimizeCurveBuilder
Default values.
Property Value CreateSketch 0 IncludePoints 1 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AngleThreshold | Returns or sets the angle threshold |
CreateSketch | Returns or sets the create sketch flag. |
CurvesToOptimize | Returns the curves and points to optimize. |
DestinationCsys | Returns or sets the destination csys as global axis. |
DistanceThreshold | Returns or sets the distance threshold |
IncludePoints | Returns or sets the include points flag. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleThreshold¶
-
OptimizeCurveBuilder.
AngleThreshold
¶ Returns or sets the angle threshold
-------------------------------------
Getter Method
Signature
AngleThreshold()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleThreshold(angleThreshold)
Parameters: angleThreshold (float) – New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateSketch¶
-
OptimizeCurveBuilder.
CreateSketch
¶ Returns or sets the create sketch flag.
If true, creates a sketch and add the optimized curves to the sketch, else doesn’t.
-------------------------------------
Getter Method
Signature
CreateSketch()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateSketch(createSketch)
Parameters: createSketch (bool) – New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CurvesToOptimize¶
-
OptimizeCurveBuilder.
CurvesToOptimize
¶ Returns the curves and points to optimize.
-------------------------------------
Getter Method
Signature
CurvesToOptimize()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX10.0.0.
License requirements: None.
DestinationCsys¶
-
OptimizeCurveBuilder.
DestinationCsys
¶ Returns or sets the destination csys as global axis.
-------------------------------------
Getter Method
Signature
DestinationCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DestinationCsys(destinationCsys)
Parameters: destinationCsys ( NXOpen.CoordinateSystem
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistanceThreshold¶
-
OptimizeCurveBuilder.
DistanceThreshold
¶ Returns or sets the distance threshold
-------------------------------------
Getter Method
Signature
DistanceThreshold()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceThreshold(distanceThreshold)
Parameters: distanceThreshold (float) – New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IncludePoints¶
-
OptimizeCurveBuilder.
IncludePoints
¶ Returns or sets the include points flag.
If true, includes points for optimization, else doesn’t
-------------------------------------
Getter Method
Signature
IncludePoints()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludePoints(includePoints)
Parameters: includePoints (bool) – New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
OptimizeCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.