OffsetMoveCurveBuilder Class¶
-
class
NXOpen.Features.
OffsetMoveCurveBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.OffsetMoveCurve
builderTo create a new instance of this class, use
NXOpen.Features.SynchronousCurveCollection.CreateOffsetMoveCurveBuilder
Default values.
Property Value CurveFinder.ChamferEnabled 0 CurveFinder.CoincidentVertexEnabled 0 CurveFinder.CollinearEnabled 0 CurveFinder.ConcentricEnabled 0 CurveFinder.EqualRadiusEnabled 0 CurveFinder.OffsetEnabled 0 CurveFinder.ParallelEnabled 0 CurveFinder.SymmetricEnabled 0 CurveFinder.TangentEnabled 0 CurveFinder.UseCurveFinder 1 CurveFinder.VertexOnCurveEnabled 0 Distance.Value 0 (millimeters part), 0 (inches part) New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CurveFinder | Returns the curve finder |
Distance | Returns the offset distance |
DistanceTolerance | Returns or sets the distance tolerance |
KeepOrthogonal | Returns or sets a value that indicates whether keep orthogonal is enabled |
KeepTangent | Returns or sets a value that indicates which keep tangent support is selected |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReverseOffsetDirection | Returns or sets the reverse offset direction |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddCurveSenseToMap | This function add the selected curve and its sense into the curve_sense_map when select a new curve |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
RemoveCurveSenseFromMap | This function remove a curve and its sense from the curve_sense_map when deselect a curve |
ReverseOffsetDirectionOfLoop | This function reverses the offset direction of the loop containing the input curve |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CurveFinder¶
-
OffsetMoveCurveBuilder.
CurveFinder
¶ Returns the curve finder
-------------------------------------
Getter Method
Signature
CurveFinder()
Returns: Return type: NXOpen.Features.CurveFinderBuilder
New in version NX9.0.0.
License requirements: None.
Distance¶
-
OffsetMoveCurveBuilder.
Distance
¶ Returns the offset distance
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
DistanceTolerance¶
-
OffsetMoveCurveBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
KeepOrthogonal¶
-
OffsetMoveCurveBuilder.
KeepOrthogonal
¶ Returns or sets a value that indicates whether keep orthogonal is enabled
-------------------------------------
Getter Method
Signature
KeepOrthogonal()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepOrthogonal(keepOrthogonal)
Parameters: keepOrthogonal (bool) – New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
KeepTangent¶
-
OffsetMoveCurveBuilder.
KeepTangent
¶ Returns or sets a value that indicates which keep tangent support is selected
-------------------------------------
Getter Method
Signature
KeepTangent()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepTangent(keepTangent)
Parameters: keepTangent (int) – New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
ReverseOffsetDirection¶
-
OffsetMoveCurveBuilder.
ReverseOffsetDirection
¶ Returns or sets the reverse offset direction
-------------------------------------
Getter Method
Signature
ReverseOffsetDirection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseOffsetDirection(reverseOffsetDirection)
Parameters: reverseOffsetDirection (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Method Detail¶
AddCurveSenseToMap¶
-
OffsetMoveCurveBuilder.
AddCurveSenseToMap
¶ This function add the selected curve and its sense into the curve_sense_map when select a new curve
Signature
AddCurveSenseToMap(curve, curveSense)
Parameters: - curve (
NXOpen.NXObject
) – A new selected curve - curveSense (int) – The sense of the selected curve
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
- curve (
RemoveCurveSenseFromMap¶
-
OffsetMoveCurveBuilder.
RemoveCurveSenseFromMap
¶ This function remove a curve and its sense from the curve_sense_map when deselect a curve
Signature
RemoveCurveSenseFromMap(curve)
Parameters: curve ( NXOpen.NXObject
) – A removed curveNew in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
ReverseOffsetDirectionOfLoop¶
-
OffsetMoveCurveBuilder.
ReverseOffsetDirectionOfLoop
¶ This function reverses the offset direction of the loop containing the input curve
Signature
ReverseOffsetDirectionOfLoop(objectInLoop)
Parameters: objectInLoop ( NXOpen.NXObject
) – A curve in loop to reverseNew in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Validate¶
-
OffsetMoveCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.