FreeformCurveCollection Class¶
-
class
NXOpen.Features.
FreeformCurveCollection
¶ Bases:
object
Collection of freeform curve based features.
To obtain an instance of this class, refer to
NXOpen.Features.FeatureCollection
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
CreatePolylineBuilder | Creates a polyline builder @return PolylineBuilder object |
CreateSmoothCurveStringBuilder | Creates a NXOpen.Features.SmoothCurveStringBuilder @return |
Method Detail¶
CreatePolylineBuilder¶
-
FreeformCurveCollection.
CreatePolylineBuilder
¶ Creates a polyline builder
Signature
CreatePolylineBuilder(polyline)
Parameters: polyline ( NXOpen.Polyline
) –NXOpen.Polyline
Returns: PolylineBuilder object Return type: NXOpen.Features.PolylineBuilder
New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
CreateSmoothCurveStringBuilder¶
-
FreeformCurveCollection.
CreateSmoothCurveStringBuilder
¶ Creates a
NXOpen.Features.SmoothCurveStringBuilder
Signature
CreateSmoothCurveStringBuilder(smoothCurveString)
Parameters: smoothCurveString ( NXOpen.Features.SmoothCurveString
) –NXOpen.Features.SmoothCurveString
to be editedReturns: Return type: NXOpen.Features.SmoothCurveStringBuilder
New in version NX9.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)