FitCurveBuilder Class¶
-
class
NXOpen.Features.
FitCurveBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.FitCurve
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateFitCurveBuilder
Default values.
Property Value Extender.EndExtensionOption None Extender.EndValue.Value 0 (millimeters part), 0 (inches part) Extender.StartExtensionOption None Extender.StartValue.Value 0 (millimeters part), 0 (inches part) IsClosedCurve true ProjectionDirectionOption Normal Radius.Value 50.0 (millimeters part), 2.0 (inches part) RejectionThreshold.Value 10.0 (millimeters part), 0.5 (inches part) New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CanKeepTemplateSelected | Returns or sets the flag indicating if template curve should be kept selected |
CanRejectPointsAutomatically | Returns or sets the flag indicating if points beyond a threshold value should be ignored during fitting |
CanUseAllPointsInPart | Returns or sets the flag indicating if all points in the part can be used for chaining |
ConstraintManager | Returns the constraint manager |
Degree | Returns or sets the degree |
Extender | Returns the extension option |
FittingParameters | Returns or sets the fitting parameters |
HasRadius | Returns or sets the has radius |
HasReversedDirection | Returns or sets the flag indicating if fitted curve direction should be reversed |
HasUniformSegments | Returns or sets the flag indicating if uniform segments should be created |
IsAssociative | Returns or sets the flag indicating if a feature should be created |
IsClosedBSpline | Returns or sets the flag indicating if a closed b-spline is to be fitted |
IsClosedCurve | Returns or sets the flag indicating if a full circle or ellipse is to be fitted |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProjectionDirection | Returns or sets the projection direction |
ProjectionDirectionOption | Returns or sets the projection direction option |
Radius | Returns the circle radius |
RejectionThreshold | Returns the rejection threshold |
Segments | Returns or sets the segments |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Target | Returns the target objects |
TargetSourceType | Returns or sets the target type |
TemplateCurve | Returns the template curve |
Tolerance | Returns or sets the tolerance |
Type | Returns or sets the type |
Methods¶
Method | Description |
---|---|
ChainAllPoints | Chains all the points in work part based on one selected point and evaluates the curve. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
DeleteTargetPoints | Deletes target points |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
Evaluate | Evaluates the curve |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetFinalTargetPoint | Returns the target point that are finally used for fitting @return |
GetFinalTargetPointsSize | Returns the number of target points that are finally used for fitting @return |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
MakeConstraint | In case of point targets, makes a target point a positional constraint. |
RemoveConstraint | Makes existing positional constraint a free target point |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
UpdateTargetSelectionOnPointEditing | Updates target selection by replacing original point by edited point. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FitCurveBuilderFittingParametersOptions Enumeration | Fitting parameters options |
FitCurveBuilderProjectionDirectionOptions Enumeration | Auxiliary curve projection direction options |
FitCurveBuilderTargetSourceTypes Enumeration | Fitting target types |
FitCurveBuilderTypes Enumeration | Fitting types |
Property Detail¶
CanKeepTemplateSelected¶
-
FitCurveBuilder.
CanKeepTemplateSelected
¶ Returns or sets the flag indicating if template curve should be kept selected
-------------------------------------
Getter Method
Signature
CanKeepTemplateSelected()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanKeepTemplateSelected(canKeepTemplateSelected)
Parameters: canKeepTemplateSelected (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CanRejectPointsAutomatically¶
-
FitCurveBuilder.
CanRejectPointsAutomatically
¶ Returns or sets the flag indicating if points beyond a threshold value should be ignored during fitting
-------------------------------------
Getter Method
Signature
CanRejectPointsAutomatically()
Returns: Return type: bool New in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
-------------------------------------
Setter Method
Signature
CanRejectPointsAutomatically(rejectPoints)
Parameters: rejectPoints (bool) – New in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
CanUseAllPointsInPart¶
-
FitCurveBuilder.
CanUseAllPointsInPart
¶ Returns or sets the flag indicating if all points in the part can be used for chaining
-------------------------------------
Getter Method
Signature
CanUseAllPointsInPart()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanUseAllPointsInPart(canUseAllPointsInPart)
Parameters: canUseAllPointsInPart (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ConstraintManager¶
-
FitCurveBuilder.
ConstraintManager
¶ Returns the constraint manager
-------------------------------------
Getter Method
Signature
ConstraintManager()
Returns: Return type: NXOpen.Features.GeometricConstraintDataManager
New in version NX8.5.0.
License requirements: None.
Degree¶
-
FitCurveBuilder.
Degree
¶ Returns or sets the degree
-------------------------------------
Getter Method
Signature
Degree()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Degree(degree)
Parameters: degree (int) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Extender¶
-
FitCurveBuilder.
Extender
¶ Returns the extension option
-------------------------------------
Getter Method
Signature
Extender()
Returns: Return type: NXOpen.GeometricUtilities.CurveExtensionBuilder
New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FittingParameters¶
-
FitCurveBuilder.
FittingParameters
¶ Returns or sets the fitting parameters
-------------------------------------
Getter Method
Signature
FittingParameters()
Returns: Return type: NXOpen.Features.FitCurveBuilderFittingParametersOptions
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FittingParameters(fittingParameters)
Parameters: fittingParameters ( NXOpen.Features.FitCurveBuilderFittingParametersOptions
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
HasRadius¶
-
FitCurveBuilder.
HasRadius
¶ Returns or sets the has radius
-------------------------------------
Getter Method
Signature
HasRadius()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HasRadius(hasRadius)
Parameters: hasRadius (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
HasReversedDirection¶
-
FitCurveBuilder.
HasReversedDirection
¶ Returns or sets the flag indicating if fitted curve direction should be reversed
-------------------------------------
Getter Method
Signature
HasReversedDirection()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HasReversedDirection(hasReversedDirection)
Parameters: hasReversedDirection (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
HasUniformSegments¶
-
FitCurveBuilder.
HasUniformSegments
¶ Returns or sets the flag indicating if uniform segments should be created
-------------------------------------
Getter Method
Signature
HasUniformSegments()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HasUniformSegments(hasUniformSegments)
Parameters: hasUniformSegments (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsAssociative¶
-
FitCurveBuilder.
IsAssociative
¶ Returns or sets the flag indicating if a feature should be created
-------------------------------------
Getter Method
Signature
IsAssociative()
Returns: Return type: bool New in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
-------------------------------------
Setter Method
Signature
IsAssociative(associative)
Parameters: associative (bool) – New in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
IsClosedBSpline¶
-
FitCurveBuilder.
IsClosedBSpline
¶ Returns or sets the flag indicating if a closed b-spline is to be fitted
-------------------------------------
Getter Method
Signature
IsClosedBSpline()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsClosedBSpline(isClosed)
Parameters: isClosed (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsClosedCurve¶
-
FitCurveBuilder.
IsClosedCurve
¶ Returns or sets the flag indicating if a full circle or ellipse is to be fitted
-------------------------------------
Getter Method
Signature
IsClosedCurve()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsClosedCurve(isClosed)
Parameters: isClosed (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ProjectionDirection¶
-
FitCurveBuilder.
ProjectionDirection
¶ Returns or sets the projection direction
-------------------------------------
Getter Method
Signature
ProjectionDirection()
Returns: Return type: NXOpen.Direction
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectionDirection(projectionDirection)
Parameters: projectionDirection ( NXOpen.Direction
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ProjectionDirectionOption¶
-
FitCurveBuilder.
ProjectionDirectionOption
¶ Returns or sets the projection direction option
-------------------------------------
Getter Method
Signature
ProjectionDirectionOption()
Returns: Return type: NXOpen.Features.FitCurveBuilderProjectionDirectionOptions
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectionDirectionOption(projectionDirectionOption)
Parameters: projectionDirectionOption ( NXOpen.Features.FitCurveBuilderProjectionDirectionOptions
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Radius¶
-
FitCurveBuilder.
Radius
¶ Returns the circle radius
-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RejectionThreshold¶
-
FitCurveBuilder.
RejectionThreshold
¶ Returns the rejection threshold
-------------------------------------
Getter Method
Signature
RejectionThreshold()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Segments¶
-
FitCurveBuilder.
Segments
¶ Returns or sets the segments
-------------------------------------
Getter Method
Signature
Segments()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Segments(segments)
Parameters: segments (int) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Target¶
-
FitCurveBuilder.
Target
¶ Returns the target objects
-------------------------------------
Getter Method
Signature
Target()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.5.0.
License requirements: None.
TargetSourceType¶
-
FitCurveBuilder.
TargetSourceType
¶ Returns or sets the target type
-------------------------------------
Getter Method
Signature
TargetSourceType()
Returns: Return type: NXOpen.Features.FitCurveBuilderTargetSourceTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetSourceType(targetSourceType)
Parameters: targetSourceType ( NXOpen.Features.FitCurveBuilderTargetSourceTypes
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TemplateCurve¶
-
FitCurveBuilder.
TemplateCurve
¶ Returns the template curve
-------------------------------------
Getter Method
Signature
TemplateCurve()
Returns: Return type: NXOpen.SelectSpline
New in version NX8.5.0.
License requirements: None.
Tolerance¶
-
FitCurveBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Type¶
-
FitCurveBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.FitCurveBuilderTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.FitCurveBuilderTypes
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
ChainAllPoints¶
-
FitCurveBuilder.
ChainAllPoints
¶ Chains all the points in work part based on one selected point and evaluates the curve.
Operation is valid for
NXOpen.Features.FitCurveBuilderTargetSourceTypes.Infer
only.Signature
ChainAllPoints()
New in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
DeleteTargetPoints¶
-
FitCurveBuilder.
DeleteTargetPoints
¶ Deletes target points
Signature
DeleteTargetPoints(points)
Parameters: points (list of NXOpen.Point
) – One of the original target points or one of the constraint manager points to remove a constraint ofNew in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
Evaluate¶
-
FitCurveBuilder.
Evaluate
¶ Evaluates the curve
Signature
Evaluate()
New in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
GetFinalTargetPoint¶
-
FitCurveBuilder.
GetFinalTargetPoint
¶ Returns the target point that are finally used for fitting
Signature
GetFinalTargetPoint(index)
Parameters: index (int) – Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
GetFinalTargetPointsSize¶
-
FitCurveBuilder.
GetFinalTargetPointsSize
¶ Returns the number of target points that are finally used for fitting
Signature
GetFinalTargetPointsSize()
Returns: Return type: int New in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
MakeConstraint¶
-
FitCurveBuilder.
MakeConstraint
¶ In case of point targets, makes a target point a positional constraint.
In case of other targets, makes one of the specified points a positional constraint
Signature
MakeConstraint(point)
Parameters: point ( NXOpen.Point
) – One of the original target points to make a constraint ofNew in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
RemoveConstraint¶
-
FitCurveBuilder.
RemoveConstraint
¶ Makes existing positional constraint a free target point
Signature
RemoveConstraint(point)
Parameters: point ( NXOpen.Point
) – One of the original target points or one of the constraint manager points to remove a constraint ofNew in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
UpdateTargetSelectionOnPointEditing¶
-
FitCurveBuilder.
UpdateTargetSelectionOnPointEditing
¶ Updates target selection by replacing original point by edited point.
When a target point is edited by dragging, the originally selected target point gets replaced by another point representing edited location. Thus it is no longer necessary for original point to remain selected.
Signature
UpdateTargetSelectionOnPointEditing()
New in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
Validate¶
-
FitCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.