ExtendSheetBuilder Class¶
-
class
NXOpen.Features.
ExtendSheetBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ExtendSheet
builderTo create a new instance of this class, use
NXOpen.Features.TrimFeatureCollection.CreateExtendSheetBuilder
Default values.
Property Value BodyOutputOption ExtendOriginalSheet CopyOriginal false LimitMethod Offset Offset.Value 5 (millimeters part), 0.2 (inches part) SideEdgeShapeOption Automatic SurfaceShapeOption NaturalCurvature New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
BodyOutputOption | Returns or sets the option to control whether the shape is extended as the original sheet, as a new face, or as a new sheet |
CopyOriginal | Returns or sets the copy original option determines if the original body is modified or a copy of the original is made |
DistanceTolerance | Returns or sets the distance tolerance |
LimitMethod | Returns or sets the option to control limit by distance or until selected objects |
LimitTools | Returns the limiting tool face or plane to extend to |
Offset | Returns the offset distance to extend |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SideEdgeShapeOption | Returns or sets the direction by which the edge is extended |
SurfaceShapeOption | Returns or sets the method by which the surface is extended which defines the shape |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetBoundaryEdges | Returns the input edges to extend |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExtendSheetBuilderBodyOutput Enumeration | Creates extension as an existing or a new entity |
ExtendSheetBuilderLimit Enumeration | Determines the Limit type for extension |
ExtendSheetBuilderSideEdgeShape Enumeration | Determines the path of the extension |
ExtendSheetBuilderSurfaceShape Enumeration | Determines the surface type of the extension |
Property Detail¶
BodyOutputOption¶
-
ExtendSheetBuilder.
BodyOutputOption
¶ Returns or sets the option to control whether the shape is extended as the original sheet, as a new face, or as a new sheet
-------------------------------------
Getter Method
Signature
BodyOutputOption()
Returns: Return type: NXOpen.Features.ExtendSheetBuilderBodyOutput
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BodyOutputOption(bodyOutputOption)
Parameters: bodyOutputOption ( NXOpen.Features.ExtendSheetBuilderBodyOutput
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CopyOriginal¶
-
ExtendSheetBuilder.
CopyOriginal
¶ Returns or sets the copy original option determines if the original body is modified or a copy of the original is made
-------------------------------------
Getter Method
Signature
CopyOriginal()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyOriginal(copyOriginal)
Parameters: copyOriginal (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistanceTolerance¶
-
ExtendSheetBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(tolerance)
Parameters: tolerance (float) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
LimitMethod¶
-
ExtendSheetBuilder.
LimitMethod
¶ Returns or sets the option to control limit by distance or until selected objects
-------------------------------------
Getter Method
Signature
LimitMethod()
Returns: Return type: NXOpen.Features.ExtendSheetBuilderLimit
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitMethod(limitMethod)
Parameters: limitMethod ( NXOpen.Features.ExtendSheetBuilderLimit
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
LimitTools¶
-
ExtendSheetBuilder.
LimitTools
¶ Returns the limiting tool face or plane to extend to
-------------------------------------
Getter Method
Signature
LimitTools()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
Offset¶
-
ExtendSheetBuilder.
Offset
¶ Returns the offset distance to extend
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
SideEdgeShapeOption¶
-
ExtendSheetBuilder.
SideEdgeShapeOption
¶ Returns or sets the direction by which the edge is extended
-------------------------------------
Getter Method
Signature
SideEdgeShapeOption()
Returns: Return type: NXOpen.Features.ExtendSheetBuilderSideEdgeShape
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SideEdgeShapeOption(sideEdgeShapeOption)
Parameters: sideEdgeShapeOption ( NXOpen.Features.ExtendSheetBuilderSideEdgeShape
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SurfaceShapeOption¶
-
ExtendSheetBuilder.
SurfaceShapeOption
¶ Returns or sets the method by which the surface is extended which defines the shape
-------------------------------------
Getter Method
Signature
SurfaceShapeOption()
Returns: Return type: NXOpen.Features.ExtendSheetBuilderSurfaceShape
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceShapeOption(surfaceShapeOption)
Parameters: surfaceShapeOption ( NXOpen.Features.ExtendSheetBuilderSurfaceShape
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TargetBoundaryEdges¶
-
ExtendSheetBuilder.
TargetBoundaryEdges
¶ Returns the input edges to extend
-------------------------------------
Getter Method
Signature
TargetBoundaryEdges()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ExtendSheetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.