ExtendSheetBuilderSurfaceShape Enumeration¶
NXOpen.Features.ExtendSheetBuilder.SurfaceShape is an alias for NXOpen.Features.ExtendSheetBuilderSurfaceShape
-
class
NXOpen.Features.
ExtendSheetBuilderSurfaceShape
¶ Bases:
object
Determines the surface type of the extension
Enum Members
Enum Member Enum Member Description NaturalCurvature Extends a B-surface with a small area that is curvature continuous at the boundary, and then tangent beyond that area.NaturalTangent Extends a B-surface tangent from the boundary.Mirrored Extends a B-surface by mirroring the curvature continuous shape of the surface.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-