ConeBuilder Class¶
-
class
NXOpen.Features.
ConeBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder for a cone feature.
This allows creation and editing of a cone feature.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateConeBuilder
Default values.
Property Value BaseDiameter.Value 50 (millimeters part), 50 (inches part) HalfAngle.Value 45 Height.Value 25 (millimeters part), 25 (inches part) TopDiameter.Value 0 (millimeters part), 0 (inches part) Type DiametersAndHeight New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Axis | Returns or sets the axis |
BaseArc | Returns the base arc |
BaseDiameter | Returns the base diameter |
BooleanOption | Returns the boolean option |
HalfAngle | Returns the half angle |
Height | Returns the height |
ParentAssociativity | Returns or sets the option to keep associativity of the cone axis |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TopArc | Returns the top arc |
TopDiameter | Returns the top diameter |
Type | Returns or sets the type represented by NXOpen.Features.ConeBuilderTypes |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConeBuilderTypes Enumeration | Represents the Cone type |
Property Detail¶
Axis¶
-
ConeBuilder.
Axis
¶ Returns or sets the axis
-------------------------------------
Getter Method
Signature
Axis()
Returns: Return type: NXOpen.Axis
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Axis(axis)
Parameters: axis ( NXOpen.Axis
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BaseArc¶
-
ConeBuilder.
BaseArc
¶ Returns the base arc
-------------------------------------
Getter Method
Signature
BaseArc()
Returns: Return type: NXOpen.SelectICurve
New in version NX6.0.0.
License requirements: None.
BaseDiameter¶
-
ConeBuilder.
BaseDiameter
¶ Returns the base diameter
-------------------------------------
Getter Method
Signature
BaseDiameter()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
BooleanOption¶
-
ConeBuilder.
BooleanOption
¶ Returns the boolean option
-------------------------------------
Getter Method
Signature
BooleanOption()
Returns: Return type: NXOpen.GeometricUtilities.BooleanOperation
New in version NX6.0.0.
License requirements: None.
HalfAngle¶
-
ConeBuilder.
HalfAngle
¶ Returns the half angle
-------------------------------------
Getter Method
Signature
HalfAngle()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Height¶
-
ConeBuilder.
Height
¶ Returns the height
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
ParentAssociativity¶
-
ConeBuilder.
ParentAssociativity
¶ Returns or sets the option to keep associativity of the cone axis
-------------------------------------
Getter Method
Signature
ParentAssociativity()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentAssociativity(parentAssociativity)
Parameters: parentAssociativity (bool) – New in version NX8.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
TopArc¶
-
ConeBuilder.
TopArc
¶ Returns the top arc
-------------------------------------
Getter Method
Signature
TopArc()
Returns: Return type: NXOpen.SelectICurve
New in version NX6.0.0.
License requirements: None.
TopDiameter¶
-
ConeBuilder.
TopDiameter
¶ Returns the top diameter
-------------------------------------
Getter Method
Signature
TopDiameter()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Type¶
-
ConeBuilder.
Type
¶ Returns or sets the type represented by
NXOpen.Features.ConeBuilderTypes
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.ConeBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.ConeBuilderTypes
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
ConeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.