ColorFeatureGroupBuilder Class¶
-
class
NXOpen.Features.
ColorFeatureGroupBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.ColorFeatureGroupBuilder
Represents a color feature group builder.The color feature group does not create a feature, but assists user to assign color to selected feature groups. To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateColorFeatureGroupBuilder
Default values.
Property Value Operation SpecifyColor Process NewFeatures New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color |
Operation | Returns or sets the color operation option. |
Process | Returns or sets the property to set color for new features only or set color and apply to all members |
SelectFeature | Returns the features to color |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ColorFeatureGroupBuilderOperationType Enumeration | specify color or remove color type |
ColorFeatureGroupBuilderProcessType Enumeration | set color for new features only or set color and apply to all members |
Property Detail¶
Color¶
-
ColorFeatureGroupBuilder.
Color
¶ Returns or sets the color
-------------------------------------
Getter Method
Signature
Color()
Returns: Return type: Id New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(color)
Parameters: color (Id) – New in version NX8.5.0.
License requirements: None.
Operation¶
-
ColorFeatureGroupBuilder.
Operation
¶ Returns or sets the color operation option.
If the option is
NXOpen.Features.ColorFeatureGroupBuilderOperationType.SpecifyColor
, assign valid color to feature. If the returned value isNXOpen.Features.ColorFeatureGroupBuilderOperationType.NoColor
, remove color from feature-------------------------------------
Getter Method
Signature
Operation()
Returns: Return type: NXOpen.Features.ColorFeatureGroupBuilderOperationType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Operation(colorOperation)
Parameters: colorOperation ( NXOpen.Features.ColorFeatureGroupBuilderOperationType
) –New in version NX8.5.0.
License requirements: None.
Process¶
-
ColorFeatureGroupBuilder.
Process
¶ Returns or sets the property to set color for new features only or set color and apply to all members
-------------------------------------
Getter Method
Signature
Process()
Returns: Return type: NXOpen.Features.ColorFeatureGroupBuilderProcessType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Process(processType)
Parameters: processType ( NXOpen.Features.ColorFeatureGroupBuilderProcessType
) –New in version NX8.5.0.
License requirements: None.
SelectFeature¶
-
ColorFeatureGroupBuilder.
SelectFeature
¶ Returns the features to color
-------------------------------------
Getter Method
Signature
SelectFeature()
Returns: Return type: NXOpen.Features.SelectFeatureList
New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
ColorFeatureGroupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.