AssociativeLineBuilder Class¶
-
class
NXOpen.Features.
AssociativeLineBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.AssociativeLine
builderTo create a new instance of this class, use
NXOpen.Features.BaseFeatureCollection.CreateAssociativeLineBuilder
Default values.
Property Value Associative True Limits.EndLimit.LimitOption AtPoint SupportPlaneData.SupportPlaneLockStatus No New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative |
EndAngle | Returns the end angle |
EndAtAngle | Returns the end at angle |
EndInferredConstraint | Returns the end inferred constraint |
EndNormal | Returns the end normal |
EndPoint | Returns the end point |
EndPointOptions | Returns or sets the end point options |
EndPointReference | Returns or sets the end point reference |
EndReferenceCsys | Returns the end reference coordinate system |
EndTangent | Returns the end tangent |
Limits | Returns the limits |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
StartAngle | Returns the start angle |
StartAtAngle | Returns the start at angle |
StartInferredConstraint | Returns the start inferred constraint |
StartNormal | Returns the start normal |
StartPoint | Returns the start point |
StartPointOptions | Returns or sets the start point options |
StartPointReference | Returns or sets the start point reference |
StartReferenceCsys | Returns the start reference coordinate system |
StartTangent | Returns the start tangent |
SupportPlaneData | Returns the support plane data |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AssociativeLineBuilderEndOption Enumeration | Represents end options type. |
AssociativeLineBuilderEndReference Enumeration | Represents references for end point |
AssociativeLineBuilderStartOption Enumeration | Represents start options type. |
AssociativeLineBuilderStartReference Enumeration | Represents references for start point |
Property Detail¶
Associative¶
-
AssociativeLineBuilder.
Associative
¶ Returns or sets the associative
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”)
EndAngle¶
-
AssociativeLineBuilder.
EndAngle
¶ Returns the end angle
-------------------------------------
Getter Method
Signature
EndAngle()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
EndAtAngle¶
-
AssociativeLineBuilder.
EndAtAngle
¶ Returns the end at angle
-------------------------------------
Getter Method
Signature
EndAtAngle()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX7.5.0.
License requirements: None.
EndInferredConstraint¶
-
AssociativeLineBuilder.
EndInferredConstraint
¶ Returns the end inferred constraint
-------------------------------------
Getter Method
Signature
EndInferredConstraint()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
EndNormal¶
-
AssociativeLineBuilder.
EndNormal
¶ Returns the end normal
-------------------------------------
Getter Method
Signature
EndNormal()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX5.0.0.
License requirements: None.
EndPoint¶
-
AssociativeLineBuilder.
EndPoint
¶ Returns the end point
-------------------------------------
Getter Method
Signature
EndPoint()
Returns: Return type: NXOpen.SelectPoint
New in version NX5.0.0.
License requirements: None.
EndPointOptions¶
-
AssociativeLineBuilder.
EndPointOptions
¶ Returns or sets the end point options
-------------------------------------
Getter Method
Signature
EndPointOptions()
Returns: Return type: NXOpen.Features.AssociativeLineBuilderEndOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPointOptions(endPointOptions)
Parameters: endPointOptions ( NXOpen.Features.AssociativeLineBuilderEndOption
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”)
EndPointReference¶
-
AssociativeLineBuilder.
EndPointReference
¶ Returns or sets the end point reference
-------------------------------------
Getter Method
Signature
EndPointReference()
Returns: Return type: NXOpen.Features.AssociativeLineBuilderEndReference
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPointReference(endPointReference)
Parameters: endPointReference ( NXOpen.Features.AssociativeLineBuilderEndReference
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”)
EndReferenceCsys¶
-
AssociativeLineBuilder.
EndReferenceCsys
¶ Returns the end reference coordinate system
-------------------------------------
Getter Method
Signature
EndReferenceCsys()
Returns: Return type: NXOpen.SelectCartesianCoordinateSystem
New in version NX5.0.0.
License requirements: None.
EndTangent¶
-
AssociativeLineBuilder.
EndTangent
¶ Returns the end tangent
-------------------------------------
Getter Method
Signature
EndTangent()
Returns: Return type: NXOpen.SelectICurve
New in version NX5.0.0.
License requirements: None.
Limits¶
-
AssociativeLineBuilder.
Limits
¶ Returns the limits
-------------------------------------
Getter Method
Signature
Limits()
Returns: Return type: NXOpen.GeometricUtilities.CurveLimitsData
New in version NX5.0.0.
License requirements: None.
StartAngle¶
-
AssociativeLineBuilder.
StartAngle
¶ Returns the start angle
-------------------------------------
Getter Method
Signature
StartAngle()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
StartAtAngle¶
-
AssociativeLineBuilder.
StartAtAngle
¶ Returns the start at angle
-------------------------------------
Getter Method
Signature
StartAtAngle()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX7.5.0.
License requirements: None.
StartInferredConstraint¶
-
AssociativeLineBuilder.
StartInferredConstraint
¶ Returns the start inferred constraint
-------------------------------------
Getter Method
Signature
StartInferredConstraint()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
StartNormal¶
-
AssociativeLineBuilder.
StartNormal
¶ Returns the start normal
-------------------------------------
Getter Method
Signature
StartNormal()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX7.5.0.
License requirements: None.
StartPoint¶
-
AssociativeLineBuilder.
StartPoint
¶ Returns the start point
-------------------------------------
Getter Method
Signature
StartPoint()
Returns: Return type: NXOpen.SelectPoint
New in version NX5.0.0.
License requirements: None.
StartPointOptions¶
-
AssociativeLineBuilder.
StartPointOptions
¶ Returns or sets the start point options
-------------------------------------
Getter Method
Signature
StartPointOptions()
Returns: Return type: NXOpen.Features.AssociativeLineBuilderStartOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPointOptions(startPointOptions)
Parameters: startPointOptions ( NXOpen.Features.AssociativeLineBuilderStartOption
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”)
StartPointReference¶
-
AssociativeLineBuilder.
StartPointReference
¶ Returns or sets the start point reference
-------------------------------------
Getter Method
Signature
StartPointReference()
Returns: Return type: NXOpen.Features.AssociativeLineBuilderStartReference
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPointReference(startPointReference)
Parameters: startPointReference ( NXOpen.Features.AssociativeLineBuilderStartReference
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”)
StartReferenceCsys¶
-
AssociativeLineBuilder.
StartReferenceCsys
¶ Returns the start reference coordinate system
-------------------------------------
Getter Method
Signature
StartReferenceCsys()
Returns: Return type: NXOpen.SelectCartesianCoordinateSystem
New in version NX5.0.0.
License requirements: None.
StartTangent¶
-
AssociativeLineBuilder.
StartTangent
¶ Returns the start tangent
-------------------------------------
Getter Method
Signature
StartTangent()
Returns: Return type: NXOpen.SelectICurve
New in version NX5.0.0.
License requirements: None.
SupportPlaneData¶
-
AssociativeLineBuilder.
SupportPlaneData
¶ Returns the support plane data
-------------------------------------
Getter Method
Signature
SupportPlaneData()
Returns: Return type: NXOpen.GeometricUtilities.SupportPlaneData
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
AssociativeLineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.