CurveLimitsData Class¶
-
class
NXOpen.GeometricUtilities.
CurveLimitsData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.CurveLimitsData
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
EndLimit | Returns the end limit |
FullCircle | Returns or sets the full circle |
StartLimit | Returns the start limit |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ComplementArc | Complements the arc |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndLimit¶
-
CurveLimitsData.
EndLimit
¶ Returns the end limit
-------------------------------------
Getter Method
Signature
EndLimit()
Returns: Return type: NXOpen.GeometricUtilities.CurveExtendData
New in version NX5.0.0.
License requirements: None.
FullCircle¶
-
CurveLimitsData.
FullCircle
¶ Returns or sets the full circle
-------------------------------------
Getter Method
Signature
FullCircle()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FullCircle(fullCircle)
Parameters: fullCircle (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”)
StartLimit¶
-
CurveLimitsData.
StartLimit
¶ Returns the start limit
-------------------------------------
Getter Method
Signature
StartLimit()
Returns: Return type: NXOpen.GeometricUtilities.CurveExtendData
New in version NX5.0.0.
License requirements: None.
Method Detail¶
ComplementArc¶
-
CurveLimitsData.
ComplementArc
¶ Complements the arc
Signature
ComplementArc()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”)
Validate¶
-
CurveLimitsData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.