ViewStyleBaseBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleBaseBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the BASE tab on the View Style Dialog (Drawings.
ViewStyleBaseBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Arrangement | Returns the arrangement on the BASE tab of the View Style Dialog |
ArrangementName | Returns or sets the arrangement name on the BASE tab of the View Style Dialog |
FacetedRepresentation | Returns or sets the faceted representation toggle on the BASE tab of the View Style Dialog |
InheritClippingBoundary | Returns or sets the inherit clipping boundary toggle on the BASE tab of the View Style Dialog |
Part | Returns or sets the part on the BASE tab of the View Style Dialog |
PartName | Returns or sets the part name on the BASE tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
TransferAnnotation | Returns or sets the transfer annotation toggle on the BASE tab of the View Style Dialog |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Arrangement¶
-
ViewStyleBaseBuilder.
Arrangement
¶ Returns the arrangement on the BASE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Arrangement()
Returns: Returns the arrangement that is on the base sub-builder Return type: NXOpen.Assemblies.ArrangementsBuilder
New in version NX6.0.0.
License requirements: None.
ArrangementName¶
-
ViewStyleBaseBuilder.
ArrangementName
¶ Returns or sets the arrangement name on the BASE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
ArrangementName()
Returns: Returns the arrangement name that is on the base sub-builder Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArrangementName(arrangementName)
Parameters: arrangementName (str) – Sets a new arrangement name on the base sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
FacetedRepresentation¶
-
ViewStyleBaseBuilder.
FacetedRepresentation
¶ Returns or sets the faceted representation toggle on the BASE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
FacetedRepresentation()
Returns: Returns the faceted representation toggle value that is on the base sub-builder Return type: bool New in version NX6.0.0.
Deprecated since version NX8.5.1: Use
Drawings.ViewStyleGeneralBuilder.ViewRepresentation
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
FacetedRepresentation(facetedRepresentationToggle)
Parameters: facetedRepresentationToggle (bool) – Sets a new faceted representation toggle value on the base sub-builder New in version NX6.0.0.
Deprecated since version NX8.5.1: Use
Drawings.ViewStyleGeneralBuilder.ViewRepresentation
instead.License requirements: drafting (“DRAFTING”)
InheritClippingBoundary¶
-
ViewStyleBaseBuilder.
InheritClippingBoundary
¶ Returns or sets the inherit clipping boundary toggle on the BASE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
InheritClippingBoundary()
Returns: Returns the inherit clipping boundary toggle value that is on the base sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritClippingBoundary(inheritClippingBoundaryToggle)
Parameters: inheritClippingBoundaryToggle (bool) – Sets a new inherit clipping boundary toggle value on the base sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Part¶
-
ViewStyleBaseBuilder.
Part
¶ Returns or sets the part on the BASE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Part()
Returns: Returns the part that is on the base sub-builder Return type: NXOpen.Part
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Part(part)
Parameters: part ( NXOpen.Part
) – Sets a new part on the base sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
PartName¶
-
ViewStyleBaseBuilder.
PartName
¶ Returns or sets the part name on the BASE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
PartName()
Returns: Returns the part name that is on the base sub-builder Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartName(partName)
Parameters: partName (str) – Sets a new part name on the base sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
TransferAnnotation¶
-
ViewStyleBaseBuilder.
TransferAnnotation
¶ Returns or sets the transfer annotation toggle on the BASE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
TransferAnnotation()
Returns: Returns the transfer annotation toggle value that is on the base sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransferAnnotation(transferAnnotationToggle)
Parameters: transferAnnotationToggle (bool) – Sets a new transfer annotation toggle value on the base sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleBaseBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.