SectionLineSettingsBuilder Class¶
-
class
NXOpen.Drawings.
SectionLineSettingsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the Section Line Settings Builder (Drawings.
SectionLineSettingsBuilder) which manages all the style attributes related * to the section Line including label letter.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ViewCommonViewLabel | Returns the view Common View label builder |
ViewSectionLine | Returns the Section Line builder |
Methods¶
Method | Description |
---|---|
InheritSettingsFromCustomerDefault | Inherit Settings From Customer Default |
InheritSettingsFromPreferences | Inherit Settings From Preference |
InheritSettingsFromSelectedObjects | Inherit Settings From Selected Objects |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ViewCommonViewLabel¶
-
SectionLineSettingsBuilder.
ViewCommonViewLabel
¶ Returns the view Common View label builder
-------------------------------------
Getter Method
Signature
ViewCommonViewLabel()
Returns: Return type: NXOpen.Drawings.ViewCommonViewLabelBuilder
New in version NX10.0.0.
License requirements: None.
ViewSectionLine¶
-
SectionLineSettingsBuilder.
ViewSectionLine
¶ Returns the Section Line builder
-------------------------------------
Getter Method
Signature
ViewSectionLine()
Returns: Return type: NXOpen.Drawings.ViewSectionLineBuilder
New in version NX10.0.0.
License requirements: None.
Method Detail¶
InheritSettingsFromCustomerDefault¶
-
SectionLineSettingsBuilder.
InheritSettingsFromCustomerDefault
¶ Inherit Settings From Customer Default
Signature
InheritSettingsFromCustomerDefault()
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
InheritSettingsFromPreferences¶
-
SectionLineSettingsBuilder.
InheritSettingsFromPreferences
¶ Inherit Settings From Preference
Signature
InheritSettingsFromPreferences()
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
InheritSettingsFromSelectedObjects¶
-
SectionLineSettingsBuilder.
InheritSettingsFromSelectedObjects
¶ Inherit Settings From Selected Objects
Signature
InheritSettingsFromSelectedObjects(selectedObject)
Parameters: selectedObject ( NXOpen.Drawings.SectionLine
) – The selected section line instance object. None is not allowed.New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
SectionLineSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.