ViewCommonViewLabelBuilder Class¶
-
class
NXOpen.Drawings.
ViewCommonViewLabelBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Drawings.ViewCommonViewLabelBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Letter | Returns or sets the letter |
SecondaryAlignment | Returns or sets the secondary alignment |
SecondaryIndexing | Returns or sets the secondary indexing |
SubscriptSizeFactor | Returns or sets the subscript size factor |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ViewCommonViewLabelBuilderSecondaryAlignmentType Enumeration | secondary Alignment Type |
ViewCommonViewLabelBuilderSecondaryIndexingType Enumeration | secondary Indexing Type |
Property Detail¶
Letter¶
-
ViewCommonViewLabelBuilder.
Letter
¶ Returns or sets the letter
-------------------------------------
Getter Method
Signature
Letter()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Letter(letter)
Parameters: letter (str) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
SecondaryAlignment¶
-
ViewCommonViewLabelBuilder.
SecondaryAlignment
¶ Returns or sets the secondary alignment
-------------------------------------
Getter Method
Signature
SecondaryAlignment()
Returns: Return type: NXOpen.Drawings.ViewCommonViewLabelBuilderSecondaryAlignmentType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondaryAlignment(secondaryAlignment)
Parameters: secondaryAlignment ( NXOpen.Drawings.ViewCommonViewLabelBuilderSecondaryAlignmentType
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
SecondaryIndexing¶
-
ViewCommonViewLabelBuilder.
SecondaryIndexing
¶ Returns or sets the secondary indexing
-------------------------------------
Getter Method
Signature
SecondaryIndexing()
Returns: Return type: NXOpen.Drawings.ViewCommonViewLabelBuilderSecondaryIndexingType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondaryIndexing(secondaryIndexing)
Parameters: secondaryIndexing ( NXOpen.Drawings.ViewCommonViewLabelBuilderSecondaryIndexingType
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
SubscriptSizeFactor¶
-
ViewCommonViewLabelBuilder.
SubscriptSizeFactor
¶ Returns or sets the subscript size factor
-------------------------------------
Getter Method
Signature
SubscriptSizeFactor()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SubscriptSizeFactor(subscriptSizeFactor)
Parameters: subscriptSizeFactor (float) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewCommonViewLabelBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.