EditViewLabelSettingsBuilder Class¶
-
class
NXOpen.Drawings.
EditViewLabelSettingsBuilder
¶ Bases:
NXOpen.Drafting.BaseEditSettingsBuilder
Represents a
NXOpen.Drawings.EditViewLabelSettingsBuilder
builder.It provides an interface for editing view label style settings. This can be used to change one specific view label or all view labels. To create a new instance of this class, use
NXOpen.Drafting.SettingsManager.CreateDrawingEditViewLabelSettingsBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AnnotationStyle | Returns the annotation style builder |
Tag | Returns the Tag for this object. |
ViewCommonViewLabel | Returns the view common view label builder |
ViewDetailLabel | Returns the view detail label builder |
ViewLabel | Returns the view label builder |
ViewProjectedLabel | Returns the view projected label builder |
ViewSectionLabel | Returns the view section label builder |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InheritSettingsFromCustomerDefault | Inherit Settings From Customer Default |
InheritSettingsFromPreferences | Inherit Settings From Preference |
InheritSettingsFromSelectedObjects | Inherit Settings From Selected Objects |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AnnotationStyle¶
-
EditViewLabelSettingsBuilder.
AnnotationStyle
¶ Returns the annotation style builder
-------------------------------------
Getter Method
Signature
AnnotationStyle()
Returns: Return type: NXOpen.Annotations.StyleBuilder
New in version NX9.0.0.
License requirements: None.
ViewCommonViewLabel¶
-
EditViewLabelSettingsBuilder.
ViewCommonViewLabel
¶ Returns the view common view label builder
-------------------------------------
Getter Method
Signature
ViewCommonViewLabel()
Returns: Return type: NXOpen.Drawings.ViewCommonViewLabelBuilder
New in version NX9.0.0.
License requirements: None.
ViewDetailLabel¶
-
EditViewLabelSettingsBuilder.
ViewDetailLabel
¶ Returns the view detail label builder
-------------------------------------
Getter Method
Signature
ViewDetailLabel()
Returns: Return type: NXOpen.Drawings.ViewDetailLabelBuilder
New in version NX9.0.0.
License requirements: None.
ViewLabel¶
-
EditViewLabelSettingsBuilder.
ViewLabel
¶ Returns the view label builder
-------------------------------------
Getter Method
Signature
ViewLabel()
Returns: Return type: NXOpen.Drawings.ViewLabelBuilder
New in version NX9.0.0.
License requirements: None.
ViewProjectedLabel¶
-
EditViewLabelSettingsBuilder.
ViewProjectedLabel
¶ Returns the view projected label builder
-------------------------------------
Getter Method
Signature
ViewProjectedLabel()
Returns: Return type: NXOpen.Drawings.ViewProjectedLabelBuilder
New in version NX9.0.0.
License requirements: None.
ViewSectionLabel¶
-
EditViewLabelSettingsBuilder.
ViewSectionLabel
¶ Returns the view section label builder
-------------------------------------
Getter Method
Signature
ViewSectionLabel()
Returns: Return type: NXOpen.Drawings.ViewSectionLabelBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
InheritSettingsFromCustomerDefault¶
-
EditViewLabelSettingsBuilder.
InheritSettingsFromCustomerDefault
¶ Inherit Settings From Customer Default
Signature
InheritSettingsFromCustomerDefault()
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
InheritSettingsFromPreferences¶
-
EditViewLabelSettingsBuilder.
InheritSettingsFromPreferences
¶ Inherit Settings From Preference
Signature
InheritSettingsFromPreferences()
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
InheritSettingsFromSelectedObjects¶
-
EditViewLabelSettingsBuilder.
InheritSettingsFromSelectedObjects
¶ Inherit Settings From Selected Objects
Signature
InheritSettingsFromSelectedObjects(selectedObject)
Parameters: selectedObject ( NXOpen.NXObject
) – The selected drafting annotation or view instance object. None is not allowed.New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
EditViewLabelSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.