ImageBasedLighting Class¶
-
class
NXOpen.Display.
ImageBasedLighting
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Display.ImageBasedLighting
Image-based Lighting (IBL) is only performed in High Quality Image renderings.IBL replaces the Lights in a scene with lighting effects derived from a given image.
This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return None.
To create a new instance of this class, use
NXOpen.ViewCollection.CreateImageBasedLighting
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Accuracy | Returns or sets the accuracy of the lighting and shadows produced from the given image |
ColorSaturation | Returns or sets the image-based lighting color saturation |
Image | Returns or sets the image-based lighting’s image builder |
ImageBlur | Returns or sets the blurr of the lighting image |
ImageFilename | Returns or sets the image filename used for image-based lighting |
ImageRotation | Returns or sets the image rotation angle (in degrees) |
ImageType | Returns or sets the image type |
ImageUpVector | Returns or sets the image up vector direction, relative to the absolute coordinate system |
ImageUpVectorType | Returns or sets the image up vector define |
Intensity | Returns or sets the intensity of the image-based lighting light effects |
LwrtAngle | Returns or sets the angle of the lwrt image-based lighting light effects |
LwrtIntensity | Returns or sets the intensity of the lwrt image-based lighting light effects |
LwrtQuality | Returns or sets the quality of the lwrt image-based lighting light effects 1 to 7 |
ShadowSoftness | Returns or sets the image-based lighting shadow softness |
ShadowType | Returns or sets the shadow type |
Tag | Returns the Tag for this object. |
UseImageBasedLighting | Returns or sets whether image-based lighting (IBL) is enabled |
UseLightsForShadowCatcherInHqi | Returns or sets whether high quality image generation (HQI) uses individual light sources or image-based lighting for shadow catcher |
UseLightsForShadowCatcherInLwrt | Returns or sets whether Advanced Studio display (lwrt) uses individual light sources or image-based lighting for shadow catcher |
UseLwrtImageBasedLighting | Returns or sets whether image-based lighting is enabled in Advanced Studio (lwrt) display |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitAndDisplay | Saves the attributes and optionally updates the display of image-based lighting |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ImageBasedLightingImageBlurType Enumeration | lighting image blurr type |
ImageBasedLightingImageUpVectorTypes Enumeration | up vector type |
ImageBasedLightingImagesType Enumeration | images type - environment used for generating image-based lighting |
ImageBasedLightingShadowsType Enumeration | shadow type |
Property Detail¶
Accuracy¶
-
ImageBasedLighting.
Accuracy
¶ Returns or sets the accuracy of the lighting and shadows produced from the given image
-------------------------------------
Getter Method
Signature
Accuracy()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Accuracy(accuracy)
Parameters: accuracy (float) – New in version NX5.0.0.
License requirements: None.
ColorSaturation¶
-
ImageBasedLighting.
ColorSaturation
¶ Returns or sets the image-based lighting color saturation
-------------------------------------
Getter Method
Signature
ColorSaturation()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorSaturation(colorSaturation)
Parameters: colorSaturation (float) – New in version NX8.5.0.
License requirements: None.
Image¶
-
ImageBasedLighting.
Image
¶ Returns or sets the image-based lighting’s image builder
-------------------------------------
Getter Method
Signature
Image()
Returns: Return type: NXOpen.Display.Image
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Image(imageBuilder)
Parameters: imageBuilder ( NXOpen.Display.Image
) –New in version NX5.0.0.
License requirements: None.
ImageBlur¶
-
ImageBasedLighting.
ImageBlur
¶ Returns or sets the blurr of the lighting image
-------------------------------------
Getter Method
Signature
ImageBlur()
Returns: Return type: NXOpen.Display.ImageBasedLightingImageBlurType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageBlur(imageBlurr)
Parameters: imageBlurr ( NXOpen.Display.ImageBasedLightingImageBlurType
) –New in version NX8.0.0.
License requirements: None.
ImageFilename¶
-
ImageBasedLighting.
ImageFilename
¶ Returns or sets the image filename used for image-based lighting
-------------------------------------
Getter Method
Signature
ImageFilename()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageFilename(imageFileName)
Parameters: imageFileName (str) – New in version NX5.0.0.
License requirements: None.
ImageRotation¶
-
ImageBasedLighting.
ImageRotation
¶ Returns or sets the image rotation angle (in degrees)
-------------------------------------
Getter Method
Signature
ImageRotation()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageRotation(imageRotation)
Parameters: imageRotation (float) – New in version NX5.0.0.
License requirements: None.
ImageType¶
-
ImageBasedLighting.
ImageType
¶ Returns or sets the image type
-------------------------------------
Getter Method
Signature
ImageType()
Returns: Return type: NXOpen.Display.ImageBasedLightingImagesType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageType(imageType)
Parameters: imageType ( NXOpen.Display.ImageBasedLightingImagesType
) –New in version NX5.0.0.
License requirements: None.
ImageUpVector¶
-
ImageBasedLighting.
ImageUpVector
¶ Returns or sets the image up vector direction, relative to the absolute coordinate system
-------------------------------------
Getter Method
Signature
ImageUpVector()
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageUpVector(imageUpVector)
Parameters: imageUpVector ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: None.
ImageUpVectorType¶
-
ImageBasedLighting.
ImageUpVectorType
¶ Returns or sets the image up vector define
-------------------------------------
Getter Method
Signature
ImageUpVectorType()
Returns: Return type: NXOpen.Display.ImageBasedLightingImageUpVectorTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageUpVectorType(imageUpVector)
Parameters: imageUpVector ( NXOpen.Display.ImageBasedLightingImageUpVectorTypes
) –New in version NX10.0.0.
License requirements: None.
Intensity¶
-
ImageBasedLighting.
Intensity
¶ Returns or sets the intensity of the image-based lighting light effects
-------------------------------------
Getter Method
Signature
Intensity()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Intensity(intensity)
Parameters: intensity (float) – New in version NX5.0.0.
License requirements: None.
LwrtAngle¶
-
ImageBasedLighting.
LwrtAngle
¶ Returns or sets the angle of the lwrt image-based lighting light effects
-------------------------------------
Getter Method
Signature
LwrtAngle()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LwrtAngle(lwrtAngle)
Parameters: lwrtAngle (float) – New in version NX8.0.0.
License requirements: None.
LwrtIntensity¶
-
ImageBasedLighting.
LwrtIntensity
¶ Returns or sets the intensity of the lwrt image-based lighting light effects
-------------------------------------
Getter Method
Signature
LwrtIntensity()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LwrtIntensity(lwrtIntensity)
Parameters: lwrtIntensity (float) – New in version NX8.0.0.
License requirements: None.
LwrtQuality¶
-
ImageBasedLighting.
LwrtQuality
¶ Returns or sets the quality of the lwrt image-based lighting light effects 1 to 7
-------------------------------------
Getter Method
Signature
LwrtQuality()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LwrtQuality(lwrtQuality)
Parameters: lwrtQuality (float) – New in version NX8.0.0.
License requirements: None.
ShadowSoftness¶
-
ImageBasedLighting.
ShadowSoftness
¶ Returns or sets the image-based lighting shadow softness
-------------------------------------
Getter Method
Signature
ShadowSoftness()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadowSoftness(shadowSoftness)
Parameters: shadowSoftness (float) – New in version NX8.5.0.
License requirements: None.
ShadowType¶
-
ImageBasedLighting.
ShadowType
¶ Returns or sets the shadow type
-------------------------------------
Getter Method
Signature
ShadowType()
Returns: Return type: NXOpen.Display.ImageBasedLightingShadowsType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadowType(shadowType)
Parameters: shadowType ( NXOpen.Display.ImageBasedLightingShadowsType
) –New in version NX5.0.0.
License requirements: None.
UseImageBasedLighting¶
-
ImageBasedLighting.
UseImageBasedLighting
¶ Returns or sets whether image-based lighting (IBL) is enabled
-------------------------------------
Getter Method
Signature
UseImageBasedLighting()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseImageBasedLighting(useIBL)
Parameters: useIBL (bool) – New in version NX5.0.0.
License requirements: None.
UseLightsForShadowCatcherInHqi¶
-
ImageBasedLighting.
UseLightsForShadowCatcherInHqi
¶ Returns or sets whether high quality image generation (HQI) uses individual light sources or image-based lighting for shadow catcher
-------------------------------------
Getter Method
Signature
UseLightsForShadowCatcherInHqi()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseLightsForShadowCatcherInHqi(useLightsForShadowCatcherInHqi)
Parameters: useLightsForShadowCatcherInHqi (bool) – New in version NX8.0.0.
License requirements: None.
UseLightsForShadowCatcherInLwrt¶
-
ImageBasedLighting.
UseLightsForShadowCatcherInLwrt
¶ Returns or sets whether Advanced Studio display (lwrt) uses individual light sources or image-based lighting for shadow catcher
-------------------------------------
Getter Method
Signature
UseLightsForShadowCatcherInLwrt()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseLightsForShadowCatcherInLwrt(useLightsForShadowCatcherInLwrt)
Parameters: useLightsForShadowCatcherInLwrt (bool) – New in version NX8.0.0.
License requirements: None.
UseLwrtImageBasedLighting¶
-
ImageBasedLighting.
UseLwrtImageBasedLighting
¶ Returns or sets whether image-based lighting is enabled in Advanced Studio (lwrt) display
-------------------------------------
Getter Method
Signature
UseLwrtImageBasedLighting()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseLwrtImageBasedLighting(useLwrtIBL)
Parameters: useLwrtIBL (bool) – New in version NX8.0.0.
License requirements: None.
Method Detail¶
CommitAndDisplay¶
-
ImageBasedLighting.
CommitAndDisplay
¶ Saves the attributes and optionally updates the display of image-based lighting
Signature
CommitAndDisplay(view, updateDisplay)
Parameters: - view (
NXOpen.View
) – View of the image-based lighting attributes - updateDisplay (bool) – True if the display should be updated
New in version NX5.0.0.
License requirements: None.
- view (
Validate¶
-
ImageBasedLighting.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.