FacetSettingsBuilder Class¶
-
class
NXOpen.Display.
FacetSettingsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Display.FacetSettingsBuilder
Facet Settings are not supported in KF.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AdvVisAlignFacets | Returns or sets the state of whether facets for advanced visualization views should be aligned along common edges. |
AdvVisFacetRatio | Returns or sets the facet ratio to use for Advanced Visualization Views |
AdvVisFacetScale | Returns or sets the facet scale to use for Advanced Visualization Views |
AdvVisFacetToViewRatio | Returns or sets the facet to view ratio to use for Advanced Visualization Views |
AdvVisRefinementFactor | Returns or sets the refinement factor to use for Advanced Visualization Views |
AdvVisTolerance | Returns or sets the tolerance setting to use for Advanced Visualization Views |
AdvVisUpdate | Returns or sets the update mode to use for Advanced Visualization Views |
ShadedAlignFacets | Returns or sets the state of whether facets for shaded views should be aligned along common edges. |
ShadedFacetRatio | Returns or sets the facet ratio to use for Shaded Views |
ShadedFacetScale | Returns or sets the facet scale to use for Shaded Views |
ShadedFacetToViewRatio | Returns or sets the facet to view ratio to use for Shaded Views |
ShadedRefinementFactor | Returns or sets the refinement factor to use for Shaded Views |
ShadedTolerance | Returns or sets the tolerance setting to use for Shaded Views |
ShadedUpdate | Returns or sets the update mode to use for Shaded Views |
ShowFacetEdges | Returns or sets the state of whether facet edges should be shown for shaded solid and sheet bodies |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAdvVisAngleTol | Returns the angle tolerance for a given tolerance set for Advanced Visualization Views @return |
GetAdvVisEdgeTol | Returns the edge tolerance for a given tolerance set for Advanced Visualization Views @return |
GetAdvVisFaceTol | Returns the face tolerance for a given tolerance set for Advanced Visualization Views @return |
GetAdvVisWidthTol | Returns the width tolerance for a given tolerance set for Advanced Visualization Views @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetShadedAngleTol | Returns the angle tolerance for a given tolerance set for Shaded Views @return |
GetShadedEdgeTol | Returns the edge tolerance for a given tolerance set for Shaded Views @return |
GetShadedFaceTol | Returns the face tolerance for a given tolerance set for Shaded Views @return |
SetAdvVisAngleTol | Sets the angle tolerance for a given tolerance set for Advanced Visualization Views |
SetAdvVisEdgeTol | Sets the edge tolerance for a given tolerance set for Advanced Visualization Views |
SetAdvVisFaceTol | Sets the face tolerance for a given tolerance set for Advanced Visualization Views |
SetAdvVisWidthTol | Sets the width tolerance for a given tolerance set for Advanced Visualization Views |
SetShadedAngleTol | Sets the angle tolerance for a given tolerance set for Shaded Views |
SetShadedEdgeTol | Sets the edge toleramce for a given tolerance set for Shaded Views |
SetShadedFaceTol | Sets the face tolerance for a given tolerance set for Shaded Views |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FacetSettingsBuilderAdvVisToleranceSetting Enumeration | Specifies which set of tolerances are to be used for rendering facets for display for Advanced Visualization views. |
FacetSettingsBuilderFacetScale Enumeration | Denotes what type of scaling factor is applied to the corresponding tolerances used to generate facets. |
FacetSettingsBuilderFacetToViewRatio Enumeration | Specifies whether the ratio of the view scale to the scale used to generate facets is determined automatically by the system (as was always done before NX 8) or whether a ratio defined by the user (by one of the set_*FacetRatio methods) is to be used as the ratio. |
FacetSettingsBuilderFacetUpdate Enumeration | Specifies whether an Update Display or Fit operation is to regenerate the facets for only visible objects, for all objects or for no objects. |
FacetSettingsBuilderShadedToleranceSetting Enumeration | Specifies which set of tolerances are to be used for rendering facets for display for Shaded views. |
Property Detail¶
AdvVisAlignFacets¶
-
FacetSettingsBuilder.
AdvVisAlignFacets
¶ Returns or sets the state of whether facets for advanced visualization views should be aligned along common edges.
Using this option will generally increase the quality of the facets but the facet generation will generally take longer.
-------------------------------------
Getter Method
Signature
AdvVisAlignFacets()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvVisAlignFacets(advVisAlignFacets)
Parameters: advVisAlignFacets (bool) – New in version NX8.5.0.
License requirements: None.
AdvVisFacetRatio¶
-
FacetSettingsBuilder.
AdvVisFacetRatio
¶ Returns or sets the facet ratio to use for Advanced Visualization Views
-------------------------------------
Getter Method
Signature
AdvVisFacetRatio()
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
NXOpen.Display.FacetSettingsBuilder.AdvVisRefinementFactor
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
AdvVisFacetRatio(advVisFacetRatio)
Parameters: advVisFacetRatio (float) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
NXOpen.Display.FacetSettingsBuilder.AdvVisRefinementFactor
insteadLicense requirements: None.
AdvVisFacetScale¶
-
FacetSettingsBuilder.
AdvVisFacetScale
¶ Returns or sets the facet scale to use for Advanced Visualization Views
-------------------------------------
Getter Method
Signature
AdvVisFacetScale()
Returns: Return type: NXOpen.Display.FacetSettingsBuilderFacetScale
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvVisFacetScale(advVisFacetScale)
Parameters: advVisFacetScale ( NXOpen.Display.FacetSettingsBuilderFacetScale
) –New in version NX9.0.0.
License requirements: None.
AdvVisFacetToViewRatio¶
-
FacetSettingsBuilder.
AdvVisFacetToViewRatio
¶ Returns or sets the facet to view ratio to use for Advanced Visualization Views
-------------------------------------
Getter Method
Signature
AdvVisFacetToViewRatio()
Returns: Return type: NXOpen.Display.FacetSettingsBuilderFacetToViewRatio
New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
NXOpen.Display.FacetSettingsBuilder.AdvVisFacetScale
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
AdvVisFacetToViewRatio(advVisFacetToViewRatio)
Parameters: advVisFacetToViewRatio ( NXOpen.Display.FacetSettingsBuilderFacetToViewRatio
) –New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
NXOpen.Display.FacetSettingsBuilder.AdvVisFacetScale
insteadLicense requirements: None.
AdvVisRefinementFactor¶
-
FacetSettingsBuilder.
AdvVisRefinementFactor
¶ Returns or sets the refinement factor to use for Advanced Visualization Views
-------------------------------------
Getter Method
Signature
AdvVisRefinementFactor()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvVisRefinementFactor(advVisRefinementFactor)
Parameters: advVisRefinementFactor (float) – New in version NX9.0.0.
License requirements: None.
AdvVisTolerance¶
-
FacetSettingsBuilder.
AdvVisTolerance
¶ Returns or sets the tolerance setting to use for Advanced Visualization Views
-------------------------------------
Getter Method
Signature
AdvVisTolerance()
Returns: Return type: NXOpen.Display.FacetSettingsBuilderAdvVisToleranceSetting
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvVisTolerance(advVisTolerance)
Parameters: advVisTolerance ( NXOpen.Display.FacetSettingsBuilderAdvVisToleranceSetting
) –New in version NX8.0.0.
License requirements: None.
AdvVisUpdate¶
-
FacetSettingsBuilder.
AdvVisUpdate
¶ Returns or sets the update mode to use for Advanced Visualization Views
-------------------------------------
Getter Method
Signature
AdvVisUpdate()
Returns: Return type: NXOpen.Display.FacetSettingsBuilderFacetUpdate
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvVisUpdate(advVisUpdate)
Parameters: advVisUpdate ( NXOpen.Display.FacetSettingsBuilderFacetUpdate
) –New in version NX8.0.0.
License requirements: None.
ShadedAlignFacets¶
-
FacetSettingsBuilder.
ShadedAlignFacets
¶ Returns or sets the state of whether facets for shaded views should be aligned along common edges.
Using this option will generally increase the quality of the facets but the facet generation will generally take longer.
-------------------------------------
Getter Method
Signature
ShadedAlignFacets()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedAlignFacets(shadedAlignFacets)
Parameters: shadedAlignFacets (bool) – New in version NX8.5.0.
License requirements: None.
ShadedFacetRatio¶
-
FacetSettingsBuilder.
ShadedFacetRatio
¶ Returns or sets the facet ratio to use for Shaded Views
-------------------------------------
Getter Method
Signature
ShadedFacetRatio()
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
NXOpen.Display.FacetSettingsBuilder.ShadedRefinementFactor
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
ShadedFacetRatio(shadedFacetRatio)
Parameters: shadedFacetRatio (float) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
NXOpen.Display.FacetSettingsBuilder.ShadedRefinementFactor
insteadLicense requirements: None.
ShadedFacetScale¶
-
FacetSettingsBuilder.
ShadedFacetScale
¶ Returns or sets the facet scale to use for Shaded Views
-------------------------------------
Getter Method
Signature
ShadedFacetScale()
Returns: Return type: NXOpen.Display.FacetSettingsBuilderFacetScale
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedFacetScale(shadedFacetScale)
Parameters: shadedFacetScale ( NXOpen.Display.FacetSettingsBuilderFacetScale
) –New in version NX9.0.0.
License requirements: None.
ShadedFacetToViewRatio¶
-
FacetSettingsBuilder.
ShadedFacetToViewRatio
¶ Returns or sets the facet to view ratio to use for Shaded Views
-------------------------------------
Getter Method
Signature
ShadedFacetToViewRatio()
Returns: Return type: NXOpen.Display.FacetSettingsBuilderFacetToViewRatio
New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
NXOpen.Display.FacetSettingsBuilder.ShadedFacetScale
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
ShadedFacetToViewRatio(shadedFacetToViewRatio)
Parameters: shadedFacetToViewRatio ( NXOpen.Display.FacetSettingsBuilderFacetToViewRatio
) –New in version NX8.0.0.
Deprecated since version NX9.0.0: Refer to
NXOpen.Display.FacetSettingsBuilder.ShadedFacetScale
insteadLicense requirements: None.
ShadedRefinementFactor¶
-
FacetSettingsBuilder.
ShadedRefinementFactor
¶ Returns or sets the refinement factor to use for Shaded Views
-------------------------------------
Getter Method
Signature
ShadedRefinementFactor()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedRefinementFactor(shadedRefinementFactor)
Parameters: shadedRefinementFactor (float) – New in version NX9.0.0.
License requirements: None.
ShadedTolerance¶
-
FacetSettingsBuilder.
ShadedTolerance
¶ Returns or sets the tolerance setting to use for Shaded Views
-------------------------------------
Getter Method
Signature
ShadedTolerance()
Returns: Return type: NXOpen.Display.FacetSettingsBuilderShadedToleranceSetting
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedTolerance(shadedTolerance)
Parameters: shadedTolerance ( NXOpen.Display.FacetSettingsBuilderShadedToleranceSetting
) –New in version NX8.0.0.
License requirements: None.
ShadedUpdate¶
-
FacetSettingsBuilder.
ShadedUpdate
¶ Returns or sets the update mode to use for Shaded Views
-------------------------------------
Getter Method
Signature
ShadedUpdate()
Returns: Return type: NXOpen.Display.FacetSettingsBuilderFacetUpdate
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedUpdate(shadedUpdate)
Parameters: shadedUpdate ( NXOpen.Display.FacetSettingsBuilderFacetUpdate
) –New in version NX8.0.0.
License requirements: None.
ShowFacetEdges¶
-
FacetSettingsBuilder.
ShowFacetEdges
¶ Returns or sets the state of whether facet edges should be shown for shaded solid and sheet bodies
-------------------------------------
Getter Method
Signature
ShowFacetEdges()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowFacetEdges(showFacetEdges)
Parameters: showFacetEdges (bool) – New in version NX8.5.0.
License requirements: None.
Method Detail¶
GetAdvVisAngleTol¶
-
FacetSettingsBuilder.
GetAdvVisAngleTol
¶ Returns the angle tolerance for a given tolerance set for Advanced Visualization Views
Signature
GetAdvVisAngleTol(advVisTolerance)
Parameters: advVisTolerance ( NXOpen.Display.FacetSettingsBuilderAdvVisToleranceSetting
) –Returns: Return type: float New in version NX8.0.0.
License requirements: None.
GetAdvVisEdgeTol¶
-
FacetSettingsBuilder.
GetAdvVisEdgeTol
¶ Returns the edge tolerance for a given tolerance set for Advanced Visualization Views
Signature
GetAdvVisEdgeTol(advVisTolerance)
Parameters: advVisTolerance ( NXOpen.Display.FacetSettingsBuilderAdvVisToleranceSetting
) –Returns: Return type: float New in version NX8.0.0.
License requirements: None.
GetAdvVisFaceTol¶
-
FacetSettingsBuilder.
GetAdvVisFaceTol
¶ Returns the face tolerance for a given tolerance set for Advanced Visualization Views
Signature
GetAdvVisFaceTol(advVisTolerance)
Parameters: advVisTolerance ( NXOpen.Display.FacetSettingsBuilderAdvVisToleranceSetting
) –Returns: Return type: float New in version NX8.0.0.
License requirements: None.
GetAdvVisWidthTol¶
-
FacetSettingsBuilder.
GetAdvVisWidthTol
¶ Returns the width tolerance for a given tolerance set for Advanced Visualization Views
Signature
GetAdvVisWidthTol(advVisTolerance)
Parameters: advVisTolerance ( NXOpen.Display.FacetSettingsBuilderAdvVisToleranceSetting
) –Returns: Return type: float New in version NX8.0.0.
License requirements: None.
GetShadedAngleTol¶
-
FacetSettingsBuilder.
GetShadedAngleTol
¶ Returns the angle tolerance for a given tolerance set for Shaded Views
Signature
GetShadedAngleTol(shadedTolerance)
Parameters: shadedTolerance ( NXOpen.Display.FacetSettingsBuilderShadedToleranceSetting
) –Returns: Return type: float New in version NX8.0.0.
License requirements: None.
GetShadedEdgeTol¶
-
FacetSettingsBuilder.
GetShadedEdgeTol
¶ Returns the edge tolerance for a given tolerance set for Shaded Views
Signature
GetShadedEdgeTol(shadedTolerance)
Parameters: shadedTolerance ( NXOpen.Display.FacetSettingsBuilderShadedToleranceSetting
) –Returns: Return type: float New in version NX8.0.0.
License requirements: None.
GetShadedFaceTol¶
-
FacetSettingsBuilder.
GetShadedFaceTol
¶ Returns the face tolerance for a given tolerance set for Shaded Views
Signature
GetShadedFaceTol(shadedTolerance)
Parameters: shadedTolerance ( NXOpen.Display.FacetSettingsBuilderShadedToleranceSetting
) –Returns: Return type: float New in version NX8.0.0.
License requirements: None.
SetAdvVisAngleTol¶
-
FacetSettingsBuilder.
SetAdvVisAngleTol
¶ Sets the angle tolerance for a given tolerance set for Advanced Visualization Views
Signature
SetAdvVisAngleTol(advVisTolerance, advVisAngleTol)
Parameters: - advVisTolerance (
NXOpen.Display.FacetSettingsBuilderAdvVisToleranceSetting
) – - advVisAngleTol (float) –
New in version NX8.0.0.
License requirements: None.
- advVisTolerance (
SetAdvVisEdgeTol¶
-
FacetSettingsBuilder.
SetAdvVisEdgeTol
¶ Sets the edge tolerance for a given tolerance set for Advanced Visualization Views
Signature
SetAdvVisEdgeTol(advVisTolerance, advVisEdgeTol)
Parameters: - advVisTolerance (
NXOpen.Display.FacetSettingsBuilderAdvVisToleranceSetting
) – - advVisEdgeTol (float) –
New in version NX8.0.0.
License requirements: None.
- advVisTolerance (
SetAdvVisFaceTol¶
-
FacetSettingsBuilder.
SetAdvVisFaceTol
¶ Sets the face tolerance for a given tolerance set for Advanced Visualization Views
Signature
SetAdvVisFaceTol(advVisTolerance, advVisFaceTol)
Parameters: - advVisTolerance (
NXOpen.Display.FacetSettingsBuilderAdvVisToleranceSetting
) – - advVisFaceTol (float) –
New in version NX8.0.0.
License requirements: None.
- advVisTolerance (
SetAdvVisWidthTol¶
-
FacetSettingsBuilder.
SetAdvVisWidthTol
¶ Sets the width tolerance for a given tolerance set for Advanced Visualization Views
Signature
SetAdvVisWidthTol(advVisTolerance, advVisWidthTol)
Parameters: - advVisTolerance (
NXOpen.Display.FacetSettingsBuilderAdvVisToleranceSetting
) – - advVisWidthTol (float) –
New in version NX8.0.0.
License requirements: None.
- advVisTolerance (
SetShadedAngleTol¶
-
FacetSettingsBuilder.
SetShadedAngleTol
¶ Sets the angle tolerance for a given tolerance set for Shaded Views
Signature
SetShadedAngleTol(shadedTolerance, shadedAngleTol)
Parameters: - shadedTolerance (
NXOpen.Display.FacetSettingsBuilderShadedToleranceSetting
) – - shadedAngleTol (float) –
New in version NX8.0.0.
License requirements: None.
- shadedTolerance (
SetShadedEdgeTol¶
-
FacetSettingsBuilder.
SetShadedEdgeTol
¶ Sets the edge toleramce for a given tolerance set for Shaded Views
Signature
SetShadedEdgeTol(shadedTolerance, shadedEdgeTol)
Parameters: - shadedTolerance (
NXOpen.Display.FacetSettingsBuilderShadedToleranceSetting
) – - shadedEdgeTol (float) –
New in version NX8.0.0.
License requirements: None.
- shadedTolerance (
SetShadedFaceTol¶
-
FacetSettingsBuilder.
SetShadedFaceTol
¶ Sets the face tolerance for a given tolerance set for Shaded Views
Signature
SetShadedFaceTol(shadedTolerance, shadedFaceTol)
Parameters: - shadedTolerance (
NXOpen.Display.FacetSettingsBuilderShadedToleranceSetting
) – - shadedFaceTol (float) –
New in version NX8.0.0.
License requirements: None.
- shadedTolerance (
Validate¶
-
FacetSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.