FacetSettingsBuilderFacetUpdate Enumeration¶
NXOpen.Display.FacetSettingsBuilder.FacetUpdate is an alias for NXOpen.Display.FacetSettingsBuilderFacetUpdate
-
class
NXOpen.Display.
FacetSettingsBuilderFacetUpdate
¶ Bases:
object
Specifies whether an Update Display or Fit operation is to regenerate the facets for only visible objects, for all objects or for no objects.
Enum Members
Enum Member Enum Member Description VisibleObjects AllObjects None -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-